Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

A tad more info on PSOC 4, attached.

   

 

   

Regards, Dana.

0 Likes
29 Replies
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Sales and product brief and order -

   

 

   

www.cypress.com/

   

 

   

Regards, Dana.

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

I'm wondering wha this 'x16' in the middle of the 4 UDBs is supposed to mean... And what 'SMX' in the analog section stands for.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

If its a $ 1.00 part we could probably assume (with < 100% certainty) that X 16 does

   

not mean 16 UDBs. Maybe each UDB is a 16 bit element/datapath ?

   

 

   

SMX, got me. Micro Digital C Object..........

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 I think it means the PSOC line will have up to 16 x UDBs.

   

with the smallest one having only have 4 UDBs

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

I don't know, the PSOC 3/5 being a $ 5 - $ 12 part, with 16 UDBs, does not

   

add up to a $ 1 part. Did M3 core dominate die area of PSOC 5, that would

   

be unusual I think.

   

 

   

Good article on M0 www.eejournal.com/archives/articles/20100105-cortex/

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

But The $1 dollar part only needs to have 4 UDBs.

   

The 16UDB PSOC 4 could cost even more than entry level PSOC5s.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

No, the $ 1 part needs to have 1024 UDBs.......yes

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 What i think is that the bottom of the line PSOC4 will e the one with only 4UDB at $1 while medium range and top of the linebe priced at $2 - $8 with more UDBs, overlaping PSOC3 and PSOC5 cost.

   

Therefore a designer with a simple application could choose the lowest priced mcu and then have a choose betwing PSOC3/PSOC4/PSOC5 as his application grows, depending on hes needs of resources and performance.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

I think I'm going to order a brand new crystal ball from my earned community points to have all those suspections cleared at once.  Cypress will, as other companies have done before, wait for the demands of the customers having placed orders in  the k's amount and talk to  their engineers. Of course everyone of us would deeply fall in love with a PSoC4 having 24 (or more) UDBs for just a buck. And if it was 2$ we would love it, too! But I think that the pricing is not realistic and competitors with FPGAs are close at Cypress's heels. Recently I was announced an M0 chip with ahhh.... hmmm..., well the basic model seemed to be something rather naked, there was a communication interface and a handfull of programmable pins for 1$. There the PSoC4 is quite a leap into my preferred direction.

   

 

   

I stay tuned

   

Bob

0 Likes
MiKO_283856
Level 4
Level 4
50 replies posted 25 replies posted 10 replies posted

 No 10 or 12-bit DAC on the horizon?

   

regards,

   

Michel

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

And MPEG4 compressor, lets keep this thread rolling 🙂

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

I heard it is time-travel capable.

0 Likes
Anonymous
Not applicable

I should clarify that the block diagram, rough pricing, and schedule describe different members of the PSoC 4 family. A detailed read of the document should provide more reliable insight.

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

1024 UDBs? Nobody will by FPGAs then, you can do anything with that 🙂

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Time travel? I would suspect that it then breaks my power budget with its 1.21Jigowatts 😞

0 Likes
MiKO_283856
Level 4
Level 4
50 replies posted 25 replies posted 10 replies posted

 Hli,

   

We should call you "Doc"

   

Regards,

   

Michel

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Oh no 

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Yeah! Doc Healy!! Would pronounce just as your provided initials! (BBS [Big Broad Smile] smileys still do not work with my ms ie browser) And for the payment of the energy, use a cable connected into the future and pay later.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

FYI - The "SMX" in the PSoC 4 architecture block diagram in the first post is the "SAR ADC MUX".

   

 

   

 

   

More official information will be released with product datasheets and specifications very shortly!

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

I would not have guessed _that_ abbreviation...

0 Likes
Anonymous
Not applicable

Hello everybody,

   

I'm completely new to the PSOC field, and hoping to learn loads! Just ordered the new dev board, and was wondering, is there a way to get email updates when more information is available for the PSOC4?

   

Thanks

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

You might be able to subsribe over at element14, but I did not look into that. AFAIK you cannot subscribe here at Cypress - you just should look maybe once a week...

   

(Actually, when you are registered at element14, you can activate email notification for a document, e.g. the Pioner Kit home page: http://www.element14.com/community/docs/DOC-53992?ICID=knode-cypresspioneerkit-space )

   

Otherwise: welcome to the wonderful and exciting world of PSoC 🙂

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

If you are using Creator now there are additionally announcements on the opening

   

page of Creator you can monitor.

   

 

   

Regards, Dana.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

You can also contact local Cypress sales office or local FAE and

   

indicate your interest in PSOC 4. It might be possible to get additional

   

info under NDA, although looks like release is imminent, so that might

   

be pointless.

   

 

   

Additionally Cypress distriubutors and their FAEs are possible sources.

   

 

   

Lastly in order to support the PSOC 4 board the Cypress Update (Software)

   

manager will invoke an update of Creator and probably Programmer to

   

support PSOC 4, so make sure you have Update Manager installed.

   

 

   

Regards, Dana.

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable
        This could be fun, The CY8C46xxx will come.   
0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable
        !   
0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

So the 4400 series seems to be the one with the many UDBs. But I wonder what "performance analog" means. Do we get just a second SAR ADC, or is there more interesting analog stuff in the pipeline?

0 Likes
Anonymous
Not applicable

Nice find. 4100 is just another mcu. The 4400 will the psoc to look up to.

   

I'm also wondering about the CY8C51LPxx, hope it finds a good price/features tradeoff

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Not exactly, you have to look at the device as a whole.
I opened up a 4100 in Creator, created 4 32 bit counters,
timing > 30 Mhz (not sure about this as enable timing,
if used as a F cntr not shown).

   



32 bit multiplier, not too shabby in a ~ $1 part.

   



The 12 bit SAR with automated mux/sampling engine front end.
I would bet a lot of DelSig designs that are configed for 16
bits are actually 10 - 12 bits when a total error analysis is
done, over temp.

   



So I recommend take a closer look, use Creator to play with
it, should lead you quickly to see 4100 can do a lot of stuff
for a $1.

   



Regards, Dana.

0 Likes