Optimal dimensions of a Capsense CSX touchpad

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
jcsb1994
Level 4
Level 4
First solution authored 50 replies posted 50 sign-ins

Hi all,

I am trying to optimize the resolution of a capsense board I have that works with a 5 by 8 CSX matrix. It works very well, with dimensions of 2.5mm electrode side length, and 0.5mm gap between each electrode

jcsb1994_1-1622836584011.png

 

jcsb1994_0-1622836391961.png

I plan on turning this into a 6x9 matrix, but I am unsure about where I should cut first:

1. should I keep the electrode size to gap distance ratio the same (i.e. make the electrodes 2mm side length and the gap 0.4mm)

2. Or should I instead reduce mainly the electrode size (i.e. 1.8mm side length with the gap kept at 0.5mm)

3. Or else should I try to optimize the electrode size and reduce the gap between them? (maybe 2.2mm side length with 0.25mm gaps)

If you can explain why one is favorable over the other, it would be perfect!!

I am asking this because I did not find any guidelines in the capsense design guide specifically for these dimensions. Please refer me to any doc if you think of any

Thank you!!

 

0 Likes
1 Solution
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

It is recommend that reduce the gap  to 0.15mm, Others are equally distributed to the length of the side.

Generally, we recommend the following sizes to our customers:

LinglingG_46_0-1623210940674.png

 

 

 

 

View solution in original post

0 Likes
4 Replies