- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm making a simple project with a custom characteristic (with read, write and notify properties enabled) where I can modify a uint8 value.
With CySmart I can connect to the psoc, and read and write the characteristic value, so everything seems fine.
To test notifications, I added a button that when pushed it triggers an interruption, in which i write to the GATT database to modify the characteristic value. So when notifications are enabled, i should see a real time value change in the characteristic when I press the button.
The problem is that when i activate notifications by writing to the CCCD and then i press the button, the characteristic value doesn't change in real time, but if then i read the characteristic value, it's correctly updated, so the button interruption works and updates the characteristic value, but the notification code doesn't notify me the changes.
I submitted the code as an attachment
- Labels:
-
BLE