Announcements

Equip yourself to optimize PSoc4 MCUs for Evs at the EV Webinar. Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

NY
Level 1
Level 1
First reply posted First question asked First like given

Hello Everyone,

I am working on a prototype development for temperature controll and data logging. Could someone help with which board I should procceed. should I select a board and add shields like in arduino or is it possible to buy a board with ethernet and modules for RTD sensors (PT100).

 

Our rough functional requiremnt is described below:

Functional Requirements
Sense Temperature T1
Sense Temperature T2
Sense Temperature T3
 
Using an algorithm to controll the following:
Control Voltage to Peltier (max 30V)
Control Current  to Peltier (max 10 A)
 
LCD Display functions 
Set Target Temperature
Show measured data as numeric values and graph
Set names for sensors (optional)
Set save frequency (save every xx seconds)
 
Data Logging:
Save sensor values as .csv Files (either through Ethernet  on to a web server or on a SD card)
T1, T2, T3, Voltage to Peltier, Current to Peltier

 

0 Likes
1 Solution
MadenoorKris
Moderator
Moderator
Moderator
50 sign-ins First like given 25 sign-ins

@NY 

Looking at your requirements, you could use any PSoC-62 eval boards. With this, you will be able to achieve SD card interface & LCD interface. The temperature sensors need to be connected to the ADC's with some signal conditioning done according to the application needs and the Peltier control loop can be implemented on the m4 core. You could use the below link to select your PSoC device by using filters and then select the available eval board:

https://www.cypress.com/products/psoc-6-microcontrollers-32-bit-arm-cortex-m4m0

We also have code examples to interface with SD card and other peripherals. Please find the link below for the examples:

https://github.com/Infineon/

https://github.com/Infineon/mtb-example-psoc6-usb-msc-filesystem-freertos

Regards,

Ram

View solution in original post

3 Replies
MadenoorKris
Moderator
Moderator
Moderator
50 sign-ins First like given 25 sign-ins

@NY 

Looking at your requirements, you could use any PSoC-62 eval boards. With this, you will be able to achieve SD card interface & LCD interface. The temperature sensors need to be connected to the ADC's with some signal conditioning done according to the application needs and the Peltier control loop can be implemented on the m4 core. You could use the below link to select your PSoC device by using filters and then select the available eval board:

https://www.cypress.com/products/psoc-6-microcontrollers-32-bit-arm-cortex-m4m0

We also have code examples to interface with SD card and other peripherals. Please find the link below for the examples:

https://github.com/Infineon/

https://github.com/Infineon/mtb-example-psoc6-usb-msc-filesystem-freertos

Regards,

Ram

NY
Level 1
Level 1
First reply posted First question asked First like given

Hi Ram,

Thank you for the response. Is it also possible to add ethernet module? so that we can configue the peltier control parameters thorugh the an IP?

it would be very helpful if we could get some support to get this off the ground.

Thank you. 

Regards,

Naresh

 

0 Likes
MadenoorKris
Moderator
Moderator
Moderator
50 sign-ins First like given 25 sign-ins

@NY 

Do you want to connect an external ethernet module to the board and get the functionality? If so, can you please mention the ethernet module part number. Also, have you previously used this module with any controller?

Regards,

Ram

0 Likes