- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Can i use LE Generate DHKey Command for CY5676A PRoC BLE 256KB Module in HCI mode ?
Because i get the status 'Unknown HCI Command' :
@15:12:38.733 <+ 50 msec> DUT command
raw = [0x01, 0x26, 0x20, 0x40, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10]
Opcode = 0x2026 (HCI_LE_GENERATE_DHKEY)
Parameter Total Length = 0x40
Remote_P_256_Public_Key = 0x100000000000000F100000000000000F100000000000000F100000000000000F100000000000000F100000000000000F100000000000000F100000000000000F
-------------------------------------------------------------------------------
@15:12:38.747 <+ 14 msec> DUT event
raw = [0x04, 0x0F, 0x04, 0x01, 0x01, 0x26, 0x20]
Event Code = 0xF (HCI_COMMAND_STATUS)
Parameter Total Length = 0x4
Status = 0x1 (Unknown HCI Command)
Num_HCI_Command_Packets = 0x1
Command_Opcode = 0x2026 (HCI_LE_GENERATE_DHKEY)
Solved! Go to Solution.
- Labels:
-
BLE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
This command is not implemented in the controller of our chip.This is implemented in the host.
Regards,
Vikas