cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

Anonymous
Not applicable

Can i use  LE Generate DHKey Command  for CY5676A PRoC BLE 256KB Module in HCI mode ?

   

Because i get the status 'Unknown HCI Command' :

   

 @15:12:38.733 <+    50 msec> DUT command
   raw = [0x01, 0x26, 0x20, 0x40, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x10]
   Opcode = 0x2026 (HCI_LE_GENERATE_DHKEY)
   Parameter Total Length = 0x40
   Remote_P_256_Public_Key = 0x100000000000000F100000000000000F100000000000000F100000000000000F100000000000000F100000000000000F100000000000000F100000000000000F
 -------------------------------------------------------------------------------
 @15:12:38.747 <+    14 msec> DUT event
   raw = [0x04, 0x0F, 0x04, 0x01, 0x01, 0x26, 0x20]
   Event Code = 0xF (HCI_COMMAND_STATUS)
   Parameter Total Length = 0x4
   Status = 0x1 (Unknown HCI Command)
   Num_HCI_Command_Packets = 0x1
   Command_Opcode = 0x2026 (HCI_LE_GENERATE_DHKEY)

0 Likes
1 Solution
Anonymous
Not applicable

Hi,

   

 

   

This command is not implemented in the controller of our chip.This is implemented in the host.

   

 

   

Regards,

   

Vikas

View solution in original post

0 Likes
2 Replies
Anonymous
Not applicable

Hi ,

   

 

   

please create a tech support case http://www.cypress.com/support?

   

 

   

Regards,

   

Vikas.

0 Likes
Anonymous
Not applicable

Hi,

   

 

   

This command is not implemented in the controller of our chip.This is implemented in the host.

   

 

   

Regards,

   

Vikas

View solution in original post

0 Likes