Hi,
I'm using a CYBLE-212006 module in combination with PSoC Creator 4.2.
I try to connect to a ble peripheral as shown in Day011_Central_Observer project from 100 Projects in 100 Days.
What does this error mean and how to fix?
Here a a code snipped:
CYBLE_GAP_BD_ADDR_T connectPeriphDevice[10];
/*
* Function Name: Get_Adv_Scan_Packets
*/
void Get_Adv_Scan_Packets(CYBLE_GAPC_ADV_REPORT_T* scanReport){
uint8 RepIndex; //Index for Bytes in Scan Response Packet {
if (devIndex < 9) {
IsDetected = 1;
// Receiving Advertisement Packet
if ((scanReport->eventType == CYBLE_GAPC_CONN_UNDIRECTED_ADV)||
(scanReport->eventType == CYBLE_GAPC_CONN_DIRECTED_ADV)||
(scanReport->eventType == CYBLE_GAPC_SCAN_UNDIRECTED_ADV)||
(scanReport->eventType == CYBLE_GAPC_NON_CONN_UNDIRECTED_ADV)){
memcpy(connectPeriphDevice[devIndex].bdAddr, scanReport->peerBdAddr,
sizeof(connectPeriphDevice[devIndex].bdAddr));
devIndex++;
}
}
else {
printf ("Device Counts Exceeds 10 \r\n");
}
}
}
//This function is called in main.c
void Handle_ble_Central_Observer_State(void) {
if (CYBLE_STACK_STATE_BUSY == CyBle_GattGetBusStatus()){
/*If stack is busy wait for ready signal*/
return;
}
if (!IsConnected) {
if(CYBLE_STATE_DISCONNECTED == CyBle_GetState()) {
if(IsSelected) {
apiResult = CyBle_GapcConnectDevice(&connectPeriphDevice[Periph_Selected]); //ERROR
if(CYBLE_ERROR_OK != apiResult ){
printf ("Connection Request to peripheral failed \r\n");
}
IsSelected = 0;
}
}
}
}
Thanks!
Pascal
Solved! Go to Solution.
Hello,
CYBLE-212006 is a Extended Range module and so this feature needs to be enabled in the code before programming. Please incorporate the following lines and it should work.
Please define the test register to switch the PA/LNA hardware control pins :
#define CYREG_SRSS_TST_DDFT_CTRL 0x40030008
Then, in the event CYBLE_EVT_STACK_ON, please include the following code snippet to enable the PA/LNA and configure the Link Layer to automatically switch PA control pin P3[2] and LNA control pin P3[3]:
case CYBLE_EVT_STACK_ON:
CY_SET_XTND_REG32((void CYFAR *)(CYREG_BLE_BLESS_RF_CONFIG), 0x0331);
CY_SET_XTND_REG32((void CYFAR *)(CYREG_SRSS_TST_DDFT_CTRL), 0x80000302);
-Sayani.
Hello,
CYBLE-212006 is a Extended Range module and so this feature needs to be enabled in the code before programming. Please incorporate the following lines and it should work.
Please define the test register to switch the PA/LNA hardware control pins :
#define CYREG_SRSS_TST_DDFT_CTRL 0x40030008
Then, in the event CYBLE_EVT_STACK_ON, please include the following code snippet to enable the PA/LNA and configure the Link Layer to automatically switch PA control pin P3[2] and LNA control pin P3[3]:
case CYBLE_EVT_STACK_ON:
CY_SET_XTND_REG32((void CYFAR *)(CYREG_BLE_BLESS_RF_CONFIG), 0x0331);
CY_SET_XTND_REG32((void CYFAR *)(CYREG_SRSS_TST_DDFT_CTRL), 0x80000302);
-Sayani.
Hi, your post is a good hint, but I already did that. Anyway, I solved the issue by just coping the ble 3.51 module from a github project into my project. I don't know the reason but in my project there was only a 3.50 version available. The component updater didn't show me any available update for this module. After the cooy process everything works fine for me! Regards Pascal