IMO clock

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
psoc_3295286
Level 4
Level 4
10 sign-ins 5 sign-ins Welcome!

Hello,

CY8C4025AZI-S413 IMO clock uses 24 MHZ frequency. But it can be changed to 48 MHz.
If it can be operated at 48MHz, then why it is rated as 24 MHz?

I want to change to CY8C4025AZI-S413 from CY8C4245AXI-483 as pins and functionality do not change much for my project.
Is it cheap to use the former?

Thank you.

0 Likes
1 Solution
PandaS
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 5 likes given

Hi @MiNe_85951 ,

You are correct, as shown in the picture attached by you: The datasheet mentions the maximum speed of the device CY8C4025AZI-S413 is 24MHz. So, the MCU cant be clocked at 48MHz by the IMO.

https://www.infineon.com/dgdl/Infineon-PSoC_4_PSoC_4000S_Datasheet_Programmable_System-on-Chip_(PSoC...

Section 7: Ordering Information

Thanks and regards,

Sobhit

View solution in original post

0 Likes
4 Replies
PandaS
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 5 likes given

Hi @psoc_3295286 ,

Yes, CY8C4025AZI-S413 (PSoC4000S Family) is an upgrade when compared to older CY8C4245AXI-483 (PSoC4200 Family). 

It has CapSense CSDv2 on PSoC 4000S family which is better in terms for performance, sensitivity and Cp Range when compared to CSDv1 on PSoC 4200 Family.

Warm regards,

Sobhit

Got it, but my question is why it is rated as 24 MHz when it can operate at 48 MHz?

Also, is it better to use CY8C4025AZI-S413 in terms of cost?

Thanks.

0 Likes
MiNe_85951
Level 7
Level 7
Distributor - TED (Japan)
50 likes received 500 replies posted 50 solutions authored

Hi,

 

The CY8C4025AZI-S413 cannot be used at 48MHz.

MaMi_1205306_0-1683883341392.png

 

MaMi_1205306_1-1683883455419.png

 

Why was the CY8C4025AZI-S413 determined to work at 48MHz?

 

Regards,

0 Likes
PandaS
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 5 likes given

Hi @MiNe_85951 ,

You are correct, as shown in the picture attached by you: The datasheet mentions the maximum speed of the device CY8C4025AZI-S413 is 24MHz. So, the MCU cant be clocked at 48MHz by the IMO.

https://www.infineon.com/dgdl/Infineon-PSoC_4_PSoC_4000S_Datasheet_Programmable_System-on-Chip_(PSoC...

Section 7: Ordering Information

Thanks and regards,

Sobhit

0 Likes