cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

Anonymous
Not applicable

Hi, this is Gaurav. I'm doing the I2c Tx project from the 101 videos. I did it several times but I'm not getting the ack signal after transmitting the protocol from the bridge.

   

I've attached the project file below. Please give the solution and explanation so that i could understand the things.

0 Likes
1 Solution
Anonymous
Not applicable

If you want to use KitProg and BCP, then you need to use I2C Pins as P3[4] and P3[5]. Check the attached project.

View solution in original post

0 Likes
2 Replies
Bob_Marlowe
Expert II

A bit more information could be helpful:

   

Which PSoC Kit do you use?

   

What code are you sending over the BCP

   

What is the exact answer?

   

What did you connect to P5_0 and P5_1

   

 

   

Did you look into your Kit's schematic to see which pins are needed for USB-I2C bridge.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

If you want to use KitProg and BCP, then you need to use I2C Pins as P3[4] and P3[5]. Check the attached project.

View solution in original post

0 Likes