- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am trying to Interface two slaves with single I2C master with my own developed board which has on CY8C4245AXI-483 controller on it.
I have interfaced two I2C slave with single master, 1. PCF8574AT usd for interfacing 20x4 LCD, 2. DS1307 RTC. i have used 4.7K resistor to make I2C lines pulls up.
what i am trying to do is to fetch data from DS1307 RTC and displaying it on LCD.
At firmware side i am using SCB block for I2C master control. When i am running my code it sending data to LCD, and LCD displaying string properly, but i am not able to Read data from DS1307 and its gives constant data.
Interesting thing is that, i have make same setup with another general purpose board with same controller chip on it which has not DS1307 on it, i have interfaced it separately and my same code is working properly with this setup.
I am not getting any idea that why its not working with my designed circuit board.
Can anyone help me to over come this problem??
Thank you.
Solved! Go to Solution.
- Tags:
- i2c problems
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
All I2C master APIs return a status which can give you a hint what runs and what not.
Can you please post your complete project or a shortened version that shows the error so that we all can have a look at all of your settings. To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.
Bob