I want to reduce the tolerance of PWM output frequency, but I don't know how.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
bugkiller
Level 2
Level 2
10 replies posted 50 sign-ins First like received

bugkiller_0-1671603862248.png

bugkiller_1-1671604076010.png

What I use : CY8CKIT-042-BLE-A

I have been a lot of fun lately while I using PSoC dev kit. But sometimes it got frustrated if ithis kind problem is occured. 

My project's input clock is 12MHz, and I want to get PWM freqeuncy which is 108kHz and 50% dutycycle. And I want to increase the frequency by 1. (108 -> 109-> 110 -> 111...)

So I configured input clock, period, compare like picture above. After finish the compiling, and I checked frequency using oscilloscope. But I only got 106kHz freq which is 2kHz less than my desired frequency. I even change to 109kHz frequency, but I only got 107kHz. Same thing happened this time.

why the frequency always 2kHz less than desired value? And how can I fix this problem?

I hope I get the answer.

 

Best regards.

0 Likes
1 Solution
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

bugkiller,

Since you are using the CY8CKIT-042-BLE-A you can use the ECO (24MHz +/- 200 ppm or better) on this kit.

Changing the PWM input clock to 24MHz here is a table of target PWM output frequency and the Period and Compare values needs to achieve the closest to the target frequencies and close to the 50% duty cycle.

Clock src=  24000000     Src tolerance =  +/- 200 ppm    
PWM Output Period Ideal Period Real Period Value PWM Freq Real Compare Ideal Compare Real Compare Value Duty Cycle Real
108000   222.2222   222 221 108108.1   111.1111   111 110 50.000%  
109000 220.1835 220 219 109090.9 110.0917 110 109 50.000%
110000 218.1818 218 217 110091.7 109.0909 109 108 50.000%
111000 216.2162 216 215 111111.1 108.1081 108 107 50.000%
112000 214.2857 214 213 112149.5 107.1429 107 106 50.000%
113000 212.3894 212 211 113207.5 106.1947 106 105 50.000%
114000 210.5263 211 210 113744.1 105.2632 105 104 49.763%
115000 208.6957 209 208 114832.5 104.3478 104 103 49.761%
116000 206.8966 207 206 115942.0 103.4483 103 102 49.758%
117000 205.1282 205 204 117073.2 102.5641 103 102 50.244%
118000 203.3898 203 202 118226.6 101.6949 102 101 50.246%
119000 201.6807 202 201 118811.9 100.8403 101 100 50.000%
120000 200.0000 200 199 120000.0 100.0000 100 99 50.000%
121000 198.3471 198 197 121212.1 99.1736 99 98 50.000%
122000 196.7213 197 196 121827.4 98.3607 98 97 49.746%
123000 195.1220 195 194 123076.9 97.5610 98 97 50.256%
124000 193.5484 194 193 123711.3 96.7742 97 96 50.000%
125000 192.0000 192 191 125000.0 96.0000 96 95 50.000%
126000 190.4762 190 189 126315.8 95.2381 95 94 50.000%
127000 188.9764 189 188 126984.1 94.4882 94 93 49.735%
128000 187.5000 188 187 127659.6 93.7500 94 93 50.000%
129000 186.0465 186 185 129032.3 93.0233 93 92 50.000%
130000 184.6154 185 184 129729.7 92.3077 92 91 49.730%

 

To achieve slightly improved target PWM output frequencies you can use the IMO at 48 MHz +/- 2%

Here's an adjusted table with the new results:

Clock src=  48000000     Src tolerance =  +/- 2%      
PWM Output Period Ideal Period Real Period Value PWM Freq Real Compare Ideal Compare Real Compare Value Duty Cycle Real
108000   444.4444   444 443 108108.1   222.2222   222 221 50.000%  
109000 440.3670 440 439 109090.9 220.1835 220 219 50.000%
110000 436.3636 436 435 110091.7 218.1818 218 217 50.000%
111000 432.4324 432 431 111111.1 216.2162 216 215 50.000%
112000 428.5714 429 428 111888.1 214.2857 214 213 49.883%
113000 424.7788 425 424 112941.2 212.3894 212 211 49.882%
114000 421.0526 421 420 114014.3 210.5263 211 210 50.119%
115000 417.3913 417 416 115107.9 208.6957 209 208 50.120%
116000 413.7931 414 413 115942.0 206.8966 207 206 50.000%
117000 410.2564 410 409 117073.2 205.1282 205 204 50.000%
118000 406.7797 407 406 117936.1 203.3898 203 202 49.877%
119000 403.3613 403 402 119106.7 201.6807 202 201 50.124%
120000 400.0000 400 399 120000.0 200.0000 200 199 50.000%
121000 396.6942 397 396 120906.8 198.3471 198 197 49.874%
122000 393.4426 393 392 122137.4 196.7213 197 196 50.127%
123000 390.2439 390 389 123076.9 195.1220 195 194 50.000%
124000 387.0968 387 386 124031.0 193.5484 194 193 50.129%
125000 384.0000 384 383 125000.0 192.0000 192 191 50.000%
126000 380.9524 381 380 125984.3 190.4762 190 189 49.869%
127000 377.9528 378 377 126984.1 188.9764 189 188 50.000%
128000 375.0000 375 374 128000.0 187.5000 188 187 50.133%
129000 372.0930 372 371 129032.3 186.0465 186 185 50.000%
130000 369.2308 369 368 130081.3 184.6154 185 184 50.136%
Len
"Engineering is an Art. The Art of Compromise."

View solution in original post

0 Likes
5 Replies
ChiP_16
Employee
Employee
5 likes given 5 solutions authored First like received

Hi bugkiller,

Based on your setting of 12MHz clock and period 111, your theoretical PWM frequency is 12MHz/(111+1) = 107.1KHz.

The PWM clock is derived from IMO clock which has a tolerance of +/- 2%. This could also contribute to the difference.

ChiP_16_0-1672377357324.png

You can use the more accurate ECO clock for HFClk (Clock1 is derived from HFClk).

ChiP_16_1-1672378239175.png

Regards,

Pong

Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

bugkiller,

Since you are using the CY8CKIT-042-BLE-A you can use the ECO (24MHz +/- 200 ppm or better) on this kit.

Changing the PWM input clock to 24MHz here is a table of target PWM output frequency and the Period and Compare values needs to achieve the closest to the target frequencies and close to the 50% duty cycle.

Clock src=  24000000     Src tolerance =  +/- 200 ppm    
PWM Output Period Ideal Period Real Period Value PWM Freq Real Compare Ideal Compare Real Compare Value Duty Cycle Real
108000   222.2222   222 221 108108.1   111.1111   111 110 50.000%  
109000 220.1835 220 219 109090.9 110.0917 110 109 50.000%
110000 218.1818 218 217 110091.7 109.0909 109 108 50.000%
111000 216.2162 216 215 111111.1 108.1081 108 107 50.000%
112000 214.2857 214 213 112149.5 107.1429 107 106 50.000%
113000 212.3894 212 211 113207.5 106.1947 106 105 50.000%
114000 210.5263 211 210 113744.1 105.2632 105 104 49.763%
115000 208.6957 209 208 114832.5 104.3478 104 103 49.761%
116000 206.8966 207 206 115942.0 103.4483 103 102 49.758%
117000 205.1282 205 204 117073.2 102.5641 103 102 50.244%
118000 203.3898 203 202 118226.6 101.6949 102 101 50.246%
119000 201.6807 202 201 118811.9 100.8403 101 100 50.000%
120000 200.0000 200 199 120000.0 100.0000 100 99 50.000%
121000 198.3471 198 197 121212.1 99.1736 99 98 50.000%
122000 196.7213 197 196 121827.4 98.3607 98 97 49.746%
123000 195.1220 195 194 123076.9 97.5610 98 97 50.256%
124000 193.5484 194 193 123711.3 96.7742 97 96 50.000%
125000 192.0000 192 191 125000.0 96.0000 96 95 50.000%
126000 190.4762 190 189 126315.8 95.2381 95 94 50.000%
127000 188.9764 189 188 126984.1 94.4882 94 93 49.735%
128000 187.5000 188 187 127659.6 93.7500 94 93 50.000%
129000 186.0465 186 185 129032.3 93.0233 93 92 50.000%
130000 184.6154 185 184 129729.7 92.3077 92 91 49.730%

 

To achieve slightly improved target PWM output frequencies you can use the IMO at 48 MHz +/- 2%

Here's an adjusted table with the new results:

Clock src=  48000000     Src tolerance =  +/- 2%      
PWM Output Period Ideal Period Real Period Value PWM Freq Real Compare Ideal Compare Real Compare Value Duty Cycle Real
108000   444.4444   444 443 108108.1   222.2222   222 221 50.000%  
109000 440.3670 440 439 109090.9 220.1835 220 219 50.000%
110000 436.3636 436 435 110091.7 218.1818 218 217 50.000%
111000 432.4324 432 431 111111.1 216.2162 216 215 50.000%
112000 428.5714 429 428 111888.1 214.2857 214 213 49.883%
113000 424.7788 425 424 112941.2 212.3894 212 211 49.882%
114000 421.0526 421 420 114014.3 210.5263 211 210 50.119%
115000 417.3913 417 416 115107.9 208.6957 209 208 50.120%
116000 413.7931 414 413 115942.0 206.8966 207 206 50.000%
117000 410.2564 410 409 117073.2 205.1282 205 204 50.000%
118000 406.7797 407 406 117936.1 203.3898 203 202 49.877%
119000 403.3613 403 402 119106.7 201.6807 202 201 50.124%
120000 400.0000 400 399 120000.0 200.0000 200 199 50.000%
121000 396.6942 397 396 120906.8 198.3471 198 197 49.874%
122000 393.4426 393 392 122137.4 196.7213 197 196 50.127%
123000 390.2439 390 389 123076.9 195.1220 195 194 50.000%
124000 387.0968 387 386 124031.0 193.5484 194 193 50.129%
125000 384.0000 384 383 125000.0 192.0000 192 191 50.000%
126000 380.9524 381 380 125984.3 190.4762 190 189 49.869%
127000 377.9528 378 377 126984.1 188.9764 189 188 50.000%
128000 375.0000 375 374 128000.0 187.5000 188 187 50.133%
129000 372.0930 372 371 129032.3 186.0465 186 185 50.000%
130000 369.2308 369 368 130081.3 184.6154 185 184 50.136%
Len
"Engineering is an Art. The Art of Compromise."
0 Likes

That is most detatiled answer that I ever get. Thanks guys!

0 Likes
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

bugkiller,

At high frequencies, the PWM output has rough granularity, so precise equidistant spacing: 108khz, 109khz, 110khz is not achievable.

To produce precise output frequencies you can use DDS component instead.

https://community.infineon.com/t5/Code-Examples/DDS24-24-bit-DDS-arbitrary-frequency-generator-compo...

DennisS_46
Employee
Employee
100 sign-ins 50 likes received 50 solutions authored

You can crank the IMO up to 48 MHz. You find that the error generally drops with higher IMO.
The plot shows the maximum error over the range of 108 to 130 kHz in absolute Hz.

DennisS_46_0-1672435380624.png

And, of course you must add in the +/- 2% error from the IMO, unless you use the ECO to achieve better precision
This gets rid of the IMO error, but not the divisor granularity.
Check out the code example as suggested by odissey1
---- Dennis

 

0 Likes