Do I have to use the function "CapSense_GetParam" instead of the function "CapSense_GetSensorCapacitance".
Or, Do I have to change something setting to be able to use the function "CapSense_GetSensorCapacitance".
Solved! Go to Solution.
Hi,
I used "CapSense_GetSensorCapacitance" with CapSense v7.0 in my sample below
void measure_caps(void)
{
CapSense_TST_MEASUREMENT_STATUS_ENUM measurementStatus ;
char str[64] ;
while(CapSense_NOT_BUSY != CapSense_IsBusy()) {
/* wait for capsent to be free */
}
TFT_BusEnable(1) ;
TFT_locate(100, 40) ;
button_cap[0] = CapSense_GetSensorCapacitance(CapSense_BUTTON0_WDGT_ID, CapSense_BUTTON0_SNS0_ID,&measurementStatus) ;
if (measurementStatus == CapSense_TST_MEASUREMENT_SUCCESS) {
snprintf(str, 64, "Button1: %d", (int)button_cap[0]) ;
TFT_putstr(str) ;
} else {
print_measure_error(measurementStatus) ;
}
TFT_locate(100, 60) ;
button_cap[1] = CapSense_GetSensorCapacitance(CapSense_BUTTON1_WDGT_ID, CapSense_BUTTON1_SNS0_ID,&measurementStatus) ;
if (measurementStatus == CapSense_TST_MEASUREMENT_SUCCESS) {
snprintf(str, 64, "Button2: %d", (int)button_cap[1]) ;
TFT_putstr(str) ;
} else {
print_measure_error(measurementStatus) ;
}
TFT_locate(100, 80) ;
button_cap[2] = CapSense_GetSensorCapacitance(CapSense_BUTTON2_WDGT_ID, CapSense_BUTTON2_SNS0_ID,&measurementStatus) ;
if (measurementStatus == CapSense_TST_MEASUREMENT_SUCCESS) {
snprintf(str, 64, "Button3: %d", (int)button_cap[2]) ;
TFT_putstr(str) ;
} else {
print_measure_error(measurementStatus) ;
}
TFT_BusEnable(0) ;
CapSense_Stop() ;
CyDelay(100) ;
CapSense_Start() ;
CapSense_ScanAllWidgets() ;
}
May be it depends on the device you are using.
I was using CY8CKIT-044 (CY8C4247AZI-M485).
moto
Hi,
I used "CapSense_GetSensorCapacitance" with CapSense v7.0 in my sample below
void measure_caps(void)
{
CapSense_TST_MEASUREMENT_STATUS_ENUM measurementStatus ;
char str[64] ;
while(CapSense_NOT_BUSY != CapSense_IsBusy()) {
/* wait for capsent to be free */
}
TFT_BusEnable(1) ;
TFT_locate(100, 40) ;
button_cap[0] = CapSense_GetSensorCapacitance(CapSense_BUTTON0_WDGT_ID, CapSense_BUTTON0_SNS0_ID,&measurementStatus) ;
if (measurementStatus == CapSense_TST_MEASUREMENT_SUCCESS) {
snprintf(str, 64, "Button1: %d", (int)button_cap[0]) ;
TFT_putstr(str) ;
} else {
print_measure_error(measurementStatus) ;
}
TFT_locate(100, 60) ;
button_cap[1] = CapSense_GetSensorCapacitance(CapSense_BUTTON1_WDGT_ID, CapSense_BUTTON1_SNS0_ID,&measurementStatus) ;
if (measurementStatus == CapSense_TST_MEASUREMENT_SUCCESS) {
snprintf(str, 64, "Button2: %d", (int)button_cap[1]) ;
TFT_putstr(str) ;
} else {
print_measure_error(measurementStatus) ;
}
TFT_locate(100, 80) ;
button_cap[2] = CapSense_GetSensorCapacitance(CapSense_BUTTON2_WDGT_ID, CapSense_BUTTON2_SNS0_ID,&measurementStatus) ;
if (measurementStatus == CapSense_TST_MEASUREMENT_SUCCESS) {
snprintf(str, 64, "Button3: %d", (int)button_cap[2]) ;
TFT_putstr(str) ;
} else {
print_measure_error(measurementStatus) ;
}
TFT_BusEnable(0) ;
CapSense_Stop() ;
CyDelay(100) ;
CapSense_Start() ;
CapSense_ScanAllWidgets() ;
}
May be it depends on the device you are using.
I was using CY8CKIT-044 (CY8C4247AZI-M485).
moto
Thank you for always helping, moto.
My device is CY8CKIT-149.
I figured out the important thing just now.
There are three selections of 'CSD tuning mode' in Configure CapSense, SmartSense(Full Auto-Tune), SmartSense(Hardware parameters only), and Manual tuning.
If I select SmartSense(Full Auto-Tune), it seems that the APIs that can be used are limited. CapSense_GetSensorCapacitance was not available.
On the other hand, If I select SmartSense(Hardware parameters only) and check 'Enable self-test library' in advanced tab I could use it.
I'm still not sure about the difference between 'Full Auto-Tune' and 'Hardware parameters only' but at any rate, CapSense_GetSensorCapacitance is now available.
I'll learn from your code and link you shared. Thank you!