cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

Anonymous
Not applicable

Hi,

I have a CY8CKIT-041-40XX kit and I want to use the on-board Kitprog2 to program an external Psoc4 chip.

I read Kitprog2 user manual on section 5.2.
It says possible but need to remove zero-ohm resistors to disconnect the onboard chip.

So I read  CY8CKIT-041-40XX Kit Guide but I can't find out which zero-ohm should be removed.

My question is how to do it on CY8CKIT-041-40XX kit.

Thanks.

0 Likes
2 Replies
Vasanth
Moderator
Moderator

Hi,

You should be able program another device even without removing the 0 ohm resistor as there are resistors in SWDIO and SWDCLK lines.

Kit schematic is available at <install_directory>\CY8CKIT-041-40XX PSoC 4 S-Series Pioneer Kit\\Hardware\CY8CKIT-041-40XX Schematic.pdf ■ <install_directory>\CY8CKIT-041-40XX PSoC 4 S-S

In that R32 is the resistor you are searching for

pastedImage_0.png

Best Regards,
VSRS

0 Likes
Anonymous
Not applicable

Hi vsrs,

Thanks for your response.

Do you mean that just connect external chip through J10? No resistor need to be unsolder.

Thanks.

0 Likes