- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I had a discussion in the thread below.
https://community.infineon.com/t5/PSoC-4/IO-Supply-Source-of-PSOC4200L/m-p/367171#M43233
I was able to use it as GPIO without clearing USBDEVv2_USBIO_CR1.IOMODE. However, when USBDEVv2_CR1.REG_ENABLE=1, the internal regulator of VBUS became active and it could not be used as a 5V interface.
When the USB port is used as 5V or 3.3V GPIO output, I would like to check if the following configuration works fine.
- USBDEVv2_USBIO_CR1.IOMODE=1 (Default)
- USBDEVv2_CR1.REG_ENABLE=0 (Default)
Is the above configuration correct when using the USB port as GPIO?
Best regards,
Inoue
- Labels:
-
PSoC 4 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @NXTY_Inoue
You have mentioned that you were able to use the USB pins as GPIO without setting the IOMODE bits in the USBDEVv2_USBIO_CR1 as 0. Can you please confirm this?
It is essential to set the IOMODE bits to 0 in order to use the USB pins as GPIOs.
The internal regulator is used to provide 3.3V to the USB D+ and D- pins in case the device is being run at 5 V (VBUS =5V). In case the device is run at 3.3V itself the internal regulator is no longer required and can remain off.
As per your question I can understand that you want to run the USB pins as GPIO but could you also confirm if you want to use the pins at 5V or 3.3V?
Best Regards
Ekta