I found that some of devices that have Bluetooth 4.0 can`t discover or can`t connect to my device but new devices can.
How to limit BLE component to 4.0 only ?
Solved! Go to Solution.
Hi Chaplin,
A Bluetooth 4.2 device can communicate with a Bluetooth 4.1 and 4.0 device(back compatible) provided that the 4.2 device does not use any Bluetooth 4.2 features.
In PSoC Creator, you can use BLE component(v3.1 and v3.2) which are Bluetooth 4.2 compatible, i.e they support the 4.2 features.
Say you have a CYBLE-222005-00, which is a 4.1 device. Now, you can still use BLE component v3.1 and v3.2. PSoC Creator knows that CYBLE-222005-00 is a 4.1 device and will return an error(and sometimes will not allow) if you try to use 4.2 features.
However if you want to restrict to Bluetooth 4.1, you will have to use older version of BLE Component, version v2.30. It is not recommended to use a older version because later versions have bug fixes and advanced features. To change version of component, right-click on project, select 'Update Components...', select v2.3 under BLE.
Hello
Can you please tell more details of the device. Please give the exact part number.
Thanks,
Hima
It`s not only one device and see other messages about this issue. This exist in Android. Because exist many versions on market I can compile with SDK to lowest version that I need. Same way Cypress must provide BLE component that can work with lowest ( 4.0) version of BLE. May be some variable for compiler #ifdef BLE_4_0 ...
Why nobody answer ? Any Cypress employers saw it ? Problem exist but nobody care about ???
Hi,
Can you please ensure that the devices that have Bluetooth 4.0 have BLE also in addition to classic bluetooth. Bluetooth 4.0 does not guarantee that BLE is also present. Our devices can be discovered only by devices that support BLE.
Regards,
-Madhu
Hi !
Please pay attention that I talk not about some device that have a problem. I asked about BLE component in PSOC Creator.
You provide it with last version 4.2 but many devices have only 4.0 or 4.1 drivers. Do you have back compatibility to old versions ?
I think must be possibility to limit code to versions of BLE.
BTW very soon BLE 5 going to arrive...
Hi Chaplin,
A Bluetooth 4.2 device can communicate with a Bluetooth 4.1 and 4.0 device(back compatible) provided that the 4.2 device does not use any Bluetooth 4.2 features.
In PSoC Creator, you can use BLE component(v3.1 and v3.2) which are Bluetooth 4.2 compatible, i.e they support the 4.2 features.
Say you have a CYBLE-222005-00, which is a 4.1 device. Now, you can still use BLE component v3.1 and v3.2. PSoC Creator knows that CYBLE-222005-00 is a 4.1 device and will return an error(and sometimes will not allow) if you try to use 4.2 features.
However if you want to restrict to Bluetooth 4.1, you will have to use older version of BLE Component, version v2.30. It is not recommended to use a older version because later versions have bug fixes and advanced features. To change version of component, right-click on project, select 'Update Components...', select v2.3 under BLE.
Thanks, I`l try but as you said in new version was bug fixes and I`l receive it ...
It must be done in component or by variable. As I said very soon you will create BLE5 component and this issue will be VERY actual.