Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
fuku_2493671
Level 1
Level 1

I've tested PSoC_4_BLE_CapSense_Proximity Project on CY8CKIT-042-BLE-A.

In this project, there are Header File "BLEApplications.h" and Source File "BLEApplications.c".

And then, I would like to transfer this project to CYBLE-222005-EVAL.

Can I use these BLEApplications files for CYBLE on PSoC Creator 4.2 ?

0 Likes
1 Solution

Hello,

Open the PSoC_4_BLE_CapSense_Proximity project. Right click - Go to Device Selector - Select CYBLE 222005-00 - Click OK. Now, program the module with this project. The target device is now changed to CYBLE 222005-00.

-Sayani.

View solution in original post

0 Likes
6 Replies
SayaniS_66
Moderator
Moderator
Moderator
10 likes received First like received

Hello,

Yes you can use the same project for CYBLE-222005-EVAL. In PSoC Creator, you need to select the module number correctly before programming. You can do so by selecting the CYBLE-222005 in the device selector option.

-Sayani.

0 Likes

I appreciate your reply.

When I select Target kit - CY8CKIT-042-BLE-A, there is Code example "PSoC_4_BLE_CapSense_Proximity".

But, when I select Target module - CYBLE-222005-00, or Target device - PRoC BLE, there is no such BLE & CapSense_Proximity example.

Do I need to update PSoC Creator 4.2?

- F.Kubo

0 Likes

Hello,

Open the PSoC_4_BLE_CapSense_Proximity project. Right click - Go to Device Selector - Select CYBLE 222005-00 - Click OK. Now, program the module with this project. The target device is now changed to CYBLE 222005-00.

-Sayani.

0 Likes

Dear Sayani,

Your changing the target device idea is very good. I tried this.

But, there is no CYBLE 222005-00 in the Device Selector. For example, there is CYBLE-214015-01.

That why, I will write BLEApplications.h and .c by myself.

I appreciate your advice!

- F.Kubo

0 Likes
lock attach
Attachments are accessible only for community members.

Hello,

I have attached a screenshot of the PSoC Creator window where you can see the CYBLE 222005-00 module.

-Sayani.

0 Likes

Hello!!

When I checked "Clear Filters" in the Device Selector, I found the CYBLE 2222005-00.

Thank you so very much!!

- F.Kubo CYBLE-222005-00.jpg

0 Likes