Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4

Len_CONSULTRON
Level 9
1000 replies posted 750 replies posted 500 likes received
Level 9

I'm using a CY8CKIT-042 in my design.  ALL my I/O is used for other purposes (LCD, SPI, LEDs and the such).  How can I detect the voltage of VDD with only internal resources?  This is to allow me to set the contract % for the LCD.

Len
"Engineering is an Art. The Art of Compromise."
0 Likes
1 Solution
Bob_Marlowe
Level 10
50 questions asked 10 questions asked 1000 solutions authored
Level 10

Have a look at the "Voltage Detect APIs" in PSoC4 System Reference Guide from Creator help menu.

Bob

PS: There is an "Edit" function to correct typos...  😉

View solution in original post

0 Likes
5 Replies
Len_CONSULTRON
Level 9
1000 replies posted 750 replies posted 500 likes received
Level 9

Update:  contrast not contract.

Len
"Engineering is an Art. The Art of Compromise."
0 Likes
Bob_Marlowe
Level 10
50 questions asked 10 questions asked 1000 solutions authored
Level 10

Have a look at the "Voltage Detect APIs" in PSoC4 System Reference Guide from Creator help menu.

Bob

PS: There is an "Edit" function to correct typos...  😉

0 Likes
Len_CONSULTRON
Level 9
1000 replies posted 750 replies posted 500 likes received
Level 9

Bob,

That was very helpful.  Although it is not an ADC (more like a comparator), I got it to work with some minor caveats.

Code snippets:

//*****************************************************************

//

uint8  vdd_voltage(void)

{

result=CY_LVD_THRESHOLD_2_50_V; //set to lowest expected VDD value

     for(result=CY_LVD_THRESHOLD_2_50_V; (result<=CY_LVD_THRESHOLD_4_50_V); result++)

     {

          CySysLvdEnable(result);

          CyDelay(10);

          if(CySysLvdGetInterruptSource() == CY_SYS_LVD_INT)

          {

          break; // If int set, break out.

          }

     }

     CySysLvdClearInterrupt();

     return(result);

}

 

lcd_contrast[] =

{

100, // CY_LVD_THRESHOLD_2_50_V

100, // CY_LVD_THRESHOLD_2_60_V

100, // CY_LVD_THRESHOLD_2_70_V

100, // CY_LVD_THRESHOLD_2_80_V

90, // CY_LVD_THRESHOLD_2_90_V

80, // CY_LVD_THRESHOLD_3_00_V

75, // CY_LVD_THRESHOLD_3_20_V

65, // CY_LVD_THRESHOLD_4_50_V

40, // > CY_LVD_THRESHOLD_4_50_V (16u)

};

 

//*****************************************************************

//

void main(void)

{

uint8  vdd_idx;

 

     CyGlobalIntEnable; /* Enable global interrupts. */

     all_LEDs(1);  /* Add load to VDD */

     LCD_Seg_Start();

     vdd_idx = vdd_voltage() - CY_LVD_THRESHOLD_2_50_V;

     LCD_Seg_SetContrast(lcd_contrast[vdd_idx]);         /* Set the contrast for VDD voltage compensation */

 

     all_LEDs(0);    /* Remove load from VDD */

...

}

CAVEATS!!!

  • The LVD thresholds aren't linear. Most are 0.1V to 0.2V steps.  The last one jumps from 3.2V to 4.5V.
  • VDD needs time to settle.  I received lower threshold/voltage values if I quickly cycle the power on and off.  That's why my code snippet includes turning on and off the LEDs (higher current draw on VDD) before and after the test.
Len
"Engineering is an Art. The Art of Compromise."
0 Likes
Vasanth
Moderator
Moderator 500 solutions authored First question asked 1000 replies posted
Moderator

Hi ,

If you have one pin free, you can use the method specified in this blog. http://www.cypress.com/blog/psoc-hacker-blog/measuring-vdd-battery-volts-psoc4  . Refer PSoC4 implementation section.

Best Regards,

VSRS

0 Likes
Len_CONSULTRON
Level 9
1000 replies posted 750 replies posted 500 likes received
Level 9

VSRS,

Thanks for your input.  I've created designs with battery voltage monitoring.  Sadly with this design, I have no spare inputs.  Yuk!  Oh well!

Len

Len
"Engineering is an Art. The Art of Compromise."
0 Likes