Attachments are accessible only for community members.
Anonymous
Not applicable
Dec 07, 2015
02:05 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dec 07, 2015
02:05 AM
Hello all,
I have coded for the simple buttons on the PSoC 4 Pioneer Board, using the onboard slider elements as Buttons. It has compiled & build OK;
Then I programmed the board, successfully. The output was tuned to respective LED's on board (Red, Yellow, Blue);
But the problem I have is:
1. It isn't holding the output i.e. I want a Toggled output but it just turns ON when touched & turns OFF when finger is removed.
What should get me out of it?
2. Also can I have Percentile illumination to the LED's @ OFF state (20%) & ON state (100%) like it was in Ez-Click?
Thanks & Regards-
Amit
7 Replies