cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

ishwariy_joshi
New Contributor II

hey! Community.

I'm facing one issue while programming CY8CKIT-145-40xxS PSoC  DevKit. I ordered CY8CKIT-145-40xxS PSoC now I'm playing with that kit I started following the User guide of that Kit. 

I performed these steps 

1) Download and installed PSoC 4 IDE

2) install Kit package from here

3) create a new blank project 

4) Select kit as shown below 

5) Compile/build project 

6) insert kit to the USB port of the laptop

7) Select the programmer  

8 )  Acquire the port 

and that point I'm getting this error.

I'm waiting for few seconds and got this message pop-up.

 

Thank you 🙂

 

 

 

Screenshot (28).png

 

 

Screenshot (31).pngScreenshot (32).png

 

 

 

 

 

 

 

 

0 Likes
1 Solution
ncbs
Moderator
Moderator

Hello @ishwariy_joshi,

Ensure that the duration of pressing SW3 is less than 5 seconds. (more explanation: Figure 1.3 in Kitprog2 user guide )

Are some other applications trying to acquire the kitprog port?
example: BCP acquiring kitprog port.

Regards,
Nikhil

View solution in original post

0 Likes
3 Replies
ncbs
Moderator
Moderator

Hello @ishwariy_joshi,

Could you press the SW3 button on your board to enter the programming mode and try again. 

Also, ensure that the SW4 switch is connected to PSoC 4000S and not to the EZ-BLE PRoC
Module.

Regards,
Nikhil

0 Likes
ishwariy_joshi
New Contributor II

@ncbs  yes I try with the SW3 button. and I already selected the Selection switch towards PSoc.

at first, I single time press the button and then trying to upload the code.

and second, try performed is press SW3 and then enter into the USB port. 

but the still issue was not solved. 

 

thank you 🙂

0 Likes
ncbs
Moderator
Moderator

Hello @ishwariy_joshi,

Ensure that the duration of pressing SW3 is less than 5 seconds. (more explanation: Figure 1.3 in Kitprog2 user guide )

Are some other applications trying to acquire the kitprog port?
example: BCP acquiring kitprog port.

Regards,
Nikhil

0 Likes