Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

Anonymous
Not applicable

Hello,

I am evaluating the CY5676A PRoC BLE 256KB Module in HCI mode. I am trying to send from the same device  two control procedures at the same time; connection update and encryption; the device process the connection update command and send the request LL_CONNECTION_UPDATE_IND when the instant is reached the LL_ENC_REQ is also send in the air.

I expect that the start encryption command is not allowed while the connection update is still no complete then the status of HCI_LE_START_ENCRYPTION should be not success?

Can anyone clarify this doubts?

pastedImage_0.png

   

Best Regards,

Message was edited by: Amina Tahiri

0 Likes
0 Replies