Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
jcsb1994
Level 4
Level 4
First solution authored 50 replies posted 50 sign-ins

Hi,

I wanted to buy a QFN PSoC 4100S Plus chip, but the only available on digikey right now is the CY8C4125LQS-423. It is not clear if I can use capsense with this chip, as the datasheet indicates a dash ( - ) on the CSD column, yet digikey says it has a capsense module.

jcsb1994_1-1633014952817.png

jcsb1994_2-1633015001300.png

I cannot validate this in the PSoC creator's device selector, as it is not even there. only the -S413 and the -S433 are available.

jcsb1994_3-1633015167794.png

 

jcsb1994_0-1633014800412.png

My question is:

1. Am I going to be able to program this chip using PSoC creator/ PSoC programmer, since I cannot pick the exact chip in the device selector?

2. Can this chip run a CSX capsense module? It is mandatory for my application.

Thanks!!

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

In Creator 4.4 the device CY8C4125LQS-S423 is shown without capsense capabilities.

 

Bob

View solution in original post

1 Reply
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

In Creator 4.4 the device CY8C4125LQS-S423 is shown without capsense capabilities.

 

Bob