Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
WaPi_297581
Level 2
Level 2
Welcome! 5 questions asked First question asked

What is required for FCC certification of a PSoC 4 BLE product?

   

A local test lab told me that if the radio has a shield, it's possible to have a specific antenna layout certified.  Then a second product could be created using an antenna having the exactl same trace width, length, board layers, board  thickness and etc. so that only emissions testing would be required.

   

 
     

0 Likes
2 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Welcome in the forum!

   

I think that you need a quite reliable answer from Cypress directly.So I would suggest you to create a "MyCase". At top of this page -> Support & Community -> Technical Support -> Create a MyCase.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Two basic parts to FCC, conducted (battery operated usually not applicable) and

   

emissions. FCC will take under consideration prior approval reference

   

material, but still performs emissions unless its a module based approach

   

where module was certified for emissions. They are very cooperative, and

   

there are approved (if my memory serves me) external labs that can assist

   

customers w/o the expertise to meet standards. I would go to their web site

   

and look for 3'rd party support.

   

 

   

    

   

          http://www.edn.com/design/systems-design/4338748/EMI-and-emissions-rules-regulations-and-options

   

 

   

Regards, Dana.

0 Likes