- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am an engineering student, I have purchased the CY8CKIT-042-BLE kit. Well, I'm new with the kit and I am trying to write a basic code to writ and read data using an I2C Master.
To write my code, I used this driver : http://www.barth-dev.de/using-the-fram-of-the-psoc-4-ble-pioneer-kit/
What I did, is that I created new project, I put an I2C Master in the schematic and I created a header file then I copied the code from FRAM.h and past it in the new header file.
in the other hand I copied the FRAM.c code and past it into the main.c (I am not sure if this is the correct way to use the driver) when I compile I do not get any errors.
Well, my question is : this is the right way to use the driver ? If yes, If I want to write a code that write and send data from Master then read it from Slave, should I open a new void main after the driver ? and which functions should I use to read and write because I'm confused with all those functions that I find in the documentation : http://www.cypress.com/file/274551/download
Thank you very much for answering,
Saban
Solved! Go to Solution.
- Labels:
-
BLE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Welcome in the forum, Mohamed.
At http://www.cypress.com/documentation/development-kitsboards/cy15framkit-001-cypresss-serial-f-ram-de... you can find the installation files for a Cypress fram kit. These include I2C examples.
The way you were building up your project was quite right, provided the given drivers from HP were correct and did not use C++.
Bob