- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I have to build a project with IAR (version 7.80.4 using a commercial license). The project is set-up with PSoC Creator 4.1 and then connected to IAR via the Project->Export to IDE. Since adding the CapSense [v4.0] component I get the following error:
Error[Li016]: size limit exceeded. The application needs 0x1a29a (107 162) bytes, which is greater than the limit of 0x8000 (32 768) bytes.
The limit is due to license "ARM.EW.LINKER" from "CapSense_SmartSense_SL_v3_10.o(Capsense_P4Library_IAR.a)" (and 1 other module).
It seems like a component (Capsense_P4Library_IAR.a) was put together with the Kickstart edition of IAR?
After taking out the CapSense component everything is fine in IAR and the application still needs more than 100kbytes.
What can I do to make it work (I have to use IAR instead of PSoC creator)?
Thanks
Thomas