Anonymous
Not applicable
Oct 04, 2016
02:11 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Oct 04, 2016
02:11 AM
Hello everyone,
I´m having a problem with notifications: the BLE event is every 30 ms, it is reading data and sending only once per event(I tried to read before, after and in the middle of two events) but my applications is time sensitive and it happens some times that the notification is not send in the next connection event and queue the notification for the second event.So, the Central device is receiving two notifications per event (it is not happening more than 20% of the time)
My question is, if there is a way to discard notifications that are not send in the nearest event and not queue it? or how a can ensure that the notification can be send in the next event?
Regards,
Edgar
Labels
- Labels:
-
BLE
2 Replies