Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

RyCo_4594291
Level 1
Level 1

I am unable to communicate to CY8KIT-148 using the MagSense tuner.  I am using example code CE222867 MagSense with Feedback LEDs and have the EZI2C component in my project.  However, when I attempt to communicate to the device using MagSense, I can only select UART and not EZI2C.  How can I fix this?

1 Solution

I was able to fix this by updating the firmware to kitprog3 by following this thread and downloading the Firmware-loader tool

View solution in original post

0 Likes
3 Replies
LinglingG_46
Moderator
Moderator
Moderator
1000 replies posted 10 questions asked 5 questions asked

Hi Ryan,

Download the CE222867 to KIT-148, then open the BCP(bridge control panel) tool. Could you list the slave address?

The I2C Bridge in Kit-148 is hardware connected.

pastedImage_0.png

0 Likes

Hello,

I have successfully programmed CE222867 and I can see the buttons and proximity sensor working as expected.  However, when I open the Bridge Control Panel, I do not see KitProg2 listed under the connected ports.  I am only able to communicate over UART and not EZI2C, which prevents me from using the MagSensAnnotation 2019-11-26 073841.pngAnnotation 2019-11-26 2.pnge tuner

0 Likes

I was able to fix this by updating the firmware to kitprog3 by following this thread and downloading the Firmware-loader tool

0 Likes