- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi to all,
I have done a simple program for testing the consumption of the EZ PRoC Module (CYBLE-022001-00). With that code the outcomes are as follows:
- Normal Mode: 12.47mA
- Deep Sleep: 1.48mA
- Hibernate: 0.24mA
The measures have been done according to the recommendations on the page 85, BLE Pioner Kit Guide for CY8CKIT-042-BLE documentation.
The code is attached. It uses Timer1 for create an interruption 5 seconds after starting. When the interruption happens, the module entries on one of the low power mode: or Deep Sleep or Hibernate, according to the mode the user has selected before the compilation and flashing.
According to the documentation (EZ-BLE PRoC Module, page 13), values should be near to the next:
- Normal Mode: 13.14mA
- Deep Sleep: 1.3uA
- Hibernate: 150nA
Does anyone could tell me why the values I have measured for low power are so far than it should be expected?
In advance, I appreciate a lot any suggestion.