- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
ERROR: address 0x82e2 of .\CortexM0\ARM_GCC_484\Debug\Reload Pro.elf section `.text' is not within region `rom'
ERROR: .\CortexM0\ARM_GCC_484\Debug\Reload Pro.elf section `.eh_frame' will not fit in region `rom'
ERROR: address 0x82e2 of .\CortexM0\ARM_GCC_484\Debug\Reload Pro.elf section `.text' is not within region `rom'
ERROR: address 0x82e2 of .\CortexM0\ARM_GCC_484\Debug\Reload Pro.elf section `.text' is not within region `rom'
ERROR: section .cyloadablemeta loaded at [00007fc0,00007fff] overlaps section .text loaded at [00001b80,000082e1]
ERROR: region `rom' overflowed by 0 bytes
collect2.exe: error: ld returned 1 exit status
The command 'arm-none-eabi-gcc.exe' failed with exit code '1'.
I have tried to refer to other cases in the community but still could not solve it. Attached please find a file for help. Best regards.
thank you
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
So from your project, I could see that your target device was CY8C4245PVI-382,
which is a 23-SSOP 32KB device.
To support your project 48KB may not be sufficient, so I would suggest to go with at least 64KB flash device.
Now to show you how to find a suitable device, please do the following steps.
(1) Go the PSoC X page, in this case PSoC 4.
From there select menu "Product Selector Guide"
(2) Then to select/organize the device selection criteria, select "Show/Hide Parameters"
(3) Then "Show/Hide Parameters" dialog will appear.
Since "Package" is in the "Hide" group as default.
Find "Package" in the "Hide" list.
(4) Drag "Package" to the "Show" and drop it (higher part will be good.)
(5) Although Flash size is in the Show list, it is placed rather in the lower position,
so I dragged it to higher position to make it easy to see both Package and Flash.
(6) Then I chose SSOP for the package. The the range for Flash was from 16KB to 32KB,
which is not enough for your current project.
(7) Then I unchecked the package, and changed the minimum requirement of Flash to 64KB.
Now you can choose a device from 171 candidates, but unfortunately there is no SSOP package available.
So please decide the most preferable package for your application and proceed.
moto