Do PSoC 4100S Max serials support IDAC?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
LeonH
Level 4
Level 4
Distributor - Arrow(GC)
100 sign-ins First solution authored 50 sign-ins

Hi Sir,

As I know, PSoC 4100S/4100S plus  support IDAC.

Does PSoC 4100S MAX not support IDAC?

Because we need to fine a solution to meet CAN FD and IDAC,

it seems psoc4 serials not support these functions in one chip.

0 Likes
1 Solution
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

@LeonH ,

I looked at Infineon's Product selection chart for the PSoC 4100s MAX product family.   It shows NO DACs.

Fourteen of these parts that have CAN, also have CAPSENSE.  I seem to remember that CAPSENSE tends to use an internal iDAC.   If so, I wonder if that iDAC can be used by the customer directly.

May I ask:  Why are you looking to use an iDAC?

Maybe an alternate circuit suggestion can be made.

Len
"Engineering is an Art. The Art of Compromise."

View solution in original post

0 Likes
1 Reply
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

@LeonH ,

I looked at Infineon's Product selection chart for the PSoC 4100s MAX product family.   It shows NO DACs.

Fourteen of these parts that have CAN, also have CAPSENSE.  I seem to remember that CAPSENSE tends to use an internal iDAC.   If so, I wonder if that iDAC can be used by the customer directly.

May I ask:  Why are you looking to use an iDAC?

Maybe an alternate circuit suggestion can be made.

Len
"Engineering is an Art. The Art of Compromise."
0 Likes