Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

JoLu_3455101
Level 4
Level 4
5 solutions authored 25 replies posted 25 sign-ins

Hi,

Cypress has a demo board for ACA-Dock application that pairs the PSoc4 with the HX3 USB3.0 hub. The purpose of the PSoC4 is to emulation different resistor values for RID:

http://www.cypress.com/documentation/other-resources/hx3-and-psoc4-based-aca-docking-solution

I have two more-specific questions in regards to this setup:

1. What kind of resistor values can the default PSoC4 firmware support/emulate? How do I select a particular value?

2. There is a note somewhere that says if additional proprietary resistor values are needed, I would need to update the PSoC4 firmware. How do I do this (i.e. which function call do I use in which section of the code)?

Thanks,

Jonathan

1 Solution
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi Jonathan,

1.The PSoC4 firmware gives no limitations on the resistor values and you can select the RID value based on the requirement of the device on the upstream port. You can simulate the RID value by either increasing the current across a lower resistance for the appropriate voltage drop across RID pin or use a multiplexer to choose between the physical resistances.

2. If you are using a physical resistor, you can use a multiplexer to choose the appropriate value and make changes to your main function which calls the Select function of the multiplexer.

Best Regards,

Sananya

View solution in original post

0 Likes
1 Reply
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi Jonathan,

1.The PSoC4 firmware gives no limitations on the resistor values and you can select the RID value based on the requirement of the device on the upstream port. You can simulate the RID value by either increasing the current across a lower resistance for the appropriate voltage drop across RID pin or use a multiplexer to choose between the physical resistances.

2. If you are using a physical resistor, you can use a multiplexer to choose the appropriate value and make changes to your main function which calls the Select function of the multiplexer.

Best Regards,

Sananya

0 Likes