Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

musac_4270856
Level 1
Level 1

Hi

Now i am going  to develop a 0 to 10 output voltage driver with multiple channels. Is there any compatible IC for it.

IC requirements are 

  • Output Voltage 0 - 10
  • Suitable for LED controllable applications
2 Replies
Yugandhar
Moderator
Moderator
Moderator
1000 replies posted 5 likes given First comment on blog

Hello,

1. For your application, you can use an IC with multiple PWMs and an external MOSFET driver instead of using DAC.

2. Please refer to the PSoC 6 MCU product in this link which has maximum of 32 TCPWM blocks.

3. You can also refer to different PSoC4200 family (maximum of 8 TCPWMs in PSoC4200L,PSoC4200M), PSoC4100 family(maximum of 8 TCPWMs in PSoC4100M,PSoC4100PS, PSoC4100S plus), PSoC4000 family(maximum of 5 TCPWMs in PSoC4000S) products in these links.

Thanks,

P Yugandhar.

0 Likes
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

safvanp,

More information is needed to help better your project, like LED type (PN, driving voltage and current), driver type (if you already decided), control type (PWM/analog), number of control outputs etc.

/odissey1

0 Likes