- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
i was wandering if there are any features of the normal PSOC 4 Pioneer kit CY8CKIT-042 that are not implemented in the CY8CKIT-042-BLE as well.
I want to start using the PSOCs and guess the PSOC Creator 101 Tutorial are a nice starting point and it is using the CY8CKIT-042, but if possible i'd like to get the BLE kit instead, so i can start playing with BLE as well after finishing the 101 for the Pioneer kit. Or are there any lessons in this 101 that cannot be done with the CY8CKIT-042-BLE kit, because it has less I/O Pin,no LED or whatsoever.
Thank you very much:)
Solved! Go to Solution.
- Labels:
-
ispn:39611:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
i was wandering if there are any features of the normal PSOC 4 Pioneer kit CY8CKIT-042 that are not implemented in the CY8CKIT-042-BLE as well.
NO.
Open a project, and do following the below steps, then you can find the different resources inside the different two chips:
1:Open a project, and right click the workspace.
2: choose different devices, then you can find the bellow list:
3: Then you can know that the CY8CKIT-042-BLE include the CY8CKIT-042 function.
4: So I think it is OK to use the CY8CKIT-042-BLE to learn the PSoC Creator 101.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
i was wandering if there are any features of the normal PSOC 4 Pioneer kit CY8CKIT-042 that are not implemented in the CY8CKIT-042-BLE as well.
NO.
Open a project, and do following the below steps, then you can find the different resources inside the different two chips:
1:Open a project, and right click the workspace.
2: choose different devices, then you can find the bellow list:
3: Then you can know that the CY8CKIT-042-BLE include the CY8CKIT-042 function.
4: So I think it is OK to use the CY8CKIT-042-BLE to learn the PSoC Creator 101.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you very much!