Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
saga_1136906
Level 3
Level 3
10 replies posted 10 questions asked 10 sign-ins

Hi,

I've a Cyble-012011-00 and I can't connect with a CYSMART 1.3. The log is:

[11:04:46:581] : 'Resolve and Set Peer Device BD Address' request sent
[11:04:46:581] : BD Address Type: PUBLIC_ADDRESS
[11:04:46:581] : BD Address: 2A:46:06:50:A0:00:00:00
[11:04:46:581] : 'Command Status' event received
[11:04:46:581] : Status: BLE_STATUS_OK
[11:04:46:581] : 'Resolve and Set Peer Device BD Address Response' event received
[11:04:46:581] : Status: 0x01
[11:04:46:581] : 'Command Complete' event received
[11:04:46:581] : Status: BLE_STATUS_OK
[11:04:46:581] : 'Establish Connection' request sent
[11:04:46:581] : BD Address Type: PUBLIC_ADDRESS
[11:04:46:581] : BD Address: 2A:46:06:50:A0:00:00:00
[11:04:46:596] : 'Command Status' event received
[11:04:46:596] : Status: BLE_STATUS_OK
[11:04:47:087] : 'Establish Connection Response' event received
[11:04:47:636] : 'Current Connection Parameters' event received
[11:04:47:636] : HCI Status: 0x00
[11:04:47:636] : Connection Interval: 8.75 ms
[11:04:47:636] : Slave Latency: 0
[11:04:47:636] : Supervision Timeout: 100 ms
[11:04:47:636] : 'Command Complete' event received
[11:04:47:636] : Status: BLE_STATUS_OK
[11:04:47:636] : 'Connection Terminated Notification' event received
[11:04:47:636] : Reason: CONNECTION_FAILED_TO_BE_ESTABLISHED
[11:04:47:636] : 'Get local device security keys' request sent
[11:04:47:761] : 'Command Status' event received
[11:04:47:761] : Status: BLE_STATUS_OK
[11:04:47:761] : 'Get local device security keys response' event received
[11:04:47:761] : Key flags: INITIATOR_ENCRYPTION_INFORMATION, INITIATOR_IDENTITY_INFORMATION, INITIATOR_SIGNATURE_KEY, RESPONDER_ENCRYPTION_INFORMATION, RESPONDER_IDENTITY_INFORMATION, RESPONDER_SIGNATURE_KEY
[11:04:47:761] : Long Term Key (LTK): [D6:93:E8:A4:23:55:48:99:1D:77:61:E6:63:2B:10:8E]
[11:04:47:761] : Encrypted Diversifier (EDIV) and Random Number: [99:1F:26:1E:F6:09:97:2E:AD:7E]
[11:04:47:761] : Identity Resolving Key (IRK): [0A:2D:F4:65:E3:BD:7B:49:1E:B4:C0:95:95:13:46:73]
[11:04:47:761] : Identification Address: [0x00A0500C082D, PUBLIC_ADDRESS]
[11:04:47:761] : Connection Signature Resolving Key (CSRK): [90:D5:06:95:92:ED:91:D7:A8:9E:2C:DC:4A:93:5B:F9]
[11:04:47:761] : 'Command Complete' event received
[11:04:47:761] : Status: BLE_STATUS_OK

Someone can't help me to solve this problem/my errors?

Thanks in advance!

0 Likes
3 Replies
Owen_Zhang123
Moderator
Moderator
Moderator
5 questions asked 500 solutions authored 250 sign-ins

Are you using the demo code or application by yourself?

Could you create the connection successfully with a demo code such as Findme Target?

0 Likes
saga_1136906
Level 3
Level 3
10 replies posted 10 questions asked 10 sign-ins

I used the demo code to be sure.

0 Likes

Which demo are you using? What's the version of your creator?

0 Likes