cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

Anonymous
Not applicable

I have a CySmart USB Dongle which I get from the Bluetooth Low Energy Pioneer Kit.

I have been using it for more than one year. Today after I connect it to the computer, the CySmart cannot found this dongle anymore. The Status LED on the dongle flash green light rapidly continuously.

What is happening?

Thank you

0 Likes
1 Solution
Anonymous
Not applicable

Pressing the reset button 5s does not work.

When I plug the dongle into the computer and open the PSoC programmer, I cannot find the dongle in the list of programmer's port. However I can upgrade the firmware of it by selecting the "Utilities" tab. So the problem solved.

View solution in original post

0 Likes
2 Replies
himam_31
Employee

Hello,

Can you verify if the device is going to the Mass Storage mode? If yes please switch it back by pressing reset switch for 5 seconds, it comes out of memory mode.

Please have a look at the KBA: Recover CySmart BLE Dongle – KBA220052

Recover CySmart BLE Dongle – KBA220052

Thanks,

Hima

0 Likes
Anonymous
Not applicable

Pressing the reset button 5s does not work.

When I plug the dongle into the computer and open the PSoC programmer, I cannot find the dongle in the list of programmer's port. However I can upgrade the firmware of it by selecting the "Utilities" tab. So the problem solved.

View solution in original post

0 Likes