Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AkFu_2553776
Level 3
Level 3
10 replies posted 5 replies posted Welcome!

Imported Cypress official example BLE_FindMe project to this device.

I can see the device name from CySmart 1.3. Connect to the device success but after following log.

Cy samrt say "Exchange GATT MTU Size timed out". If comment out Line 215 to 243 then works without these problem.

These lines are BLE sleep related.

Attached both project file.

How Can I make BLE work with sleep functions?

[12:10:34:761] : 'Establish Connection' request sent

[12:10:34:761] : BD Address Type: PUBLIC_ADDRESS

[12:10:34:761] : BD Address: 03:00:00:50:A0:00:00:00

[12:10:34:764] : 'Command Status' event received

[12:10:34:764] : Status: BLE_STATUS_OK

[12:10:34:811] : 'Establish Connection Response' event received

[12:10:35:794] : 'Current Connection Parameters' event received

[12:10:35:794] : HCI Status: 0x00

[12:10:35:794] : Connection Interval: 8.75 ms

[12:10:35:794] : Slave Latency: 0

[12:10:35:794] : Supervision Timeout: 100 ms

[12:10:35:794] : 'Command Complete' event received

[12:10:35:794] : Status: BLE_STATUS_OK

[12:10:35:795] : 'Get local device security keys' request sent

[12:10:35:796] : 'Command Status' event received

[12:10:35:796] : Status: BLE_STATUS_OK

[12:10:35:803] : 'Get local device security keys response' event received

[12:10:35:803] : Key flags: INITIATOR_ENCRYPTION_INFORMATION, INITIATOR_IDENTITY_INFORMATION, INITIATOR_SIGNATURE_KEY, RESPONDER_ENCRYPTION_INFORMATION, RESPONDER_IDENTITY_INFORMATION, RESPONDER_SIGNATURE_KEY

[12:10:35:803] : Long Term Key (LTK): [D6:93:E8:A4:23:55:48:99:1D:77:61:E6:63:2B:10:8E]

[12:10:35:803] : Encrypted Diversifier (EDIV) and Random Number: [99:1F:26:1E:F6:09:97:2E:AD:7E]

[12:10:35:803] : Identity Resolving Key (IRK): [0A:2D:F4:65:E3:BD:7B:49:1E:B4:C0:95:95:13:46:73]

[12:10:35:803] : Identification Address: [0x00A0500C1313, PUBLIC_ADDRESS]

[12:10:35:803] : Connection Signature Resolving Key (CSRK): [90:D5:06:95:92:ED:91:D7:A8:9E:2C:DC:4A:93:5B:F9]

[12:10:35:804] : 'Command Complete' event received

[12:10:35:804] : Status: BLE_STATUS_OK

[12:10:35:804] : 'Set OOB data' request sent

[12:10:35:804] : OOB flag: Disable

[12:10:35:804] : OOB Key: [00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00]

[12:10:35:804] : OOB Data: [00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00]

[12:10:35:809] : 'Command Status' event received

[12:10:35:809] : Status: BLE_STATUS_OK

[12:10:35:810] : 'Command Complete' event received

[12:10:35:810] : Status: BLE_STATUS_OK

[12:10:35:810] : 'Exchange GATT MTU Size' request sent

[12:10:35:810] : MTU: 0x0200

[12:10:35:813] : 'Command Status' event received

[12:10:35:813] : Status: BLE_STATUS_OK

1 Solution

Hi Ganesh.

Removed ECO's external capacitors made them work.

Thanks,

Aki

View solution in original post

0 Likes
2 Replies
VenkataD_41
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi,

I am not able to reproduce the issue at my end. I am not able to see the error "Exchange GATT MTU Size timed out" at my side. I am using the kit CY8CKIT-042-BLE baseboard with CY8C4248LQI-BL583 EVAL board. Please let me know what board you are using at your end to reproduce the same.

Thanks

Ganesh

0 Likes

Hi Ganesh.

Removed ECO's external capacitors made them work.

Thanks,

Aki

0 Likes