Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

patrick1957
Level 1
First reply posted First question asked Welcome!
Level 1

Hi,

I'm using "CY8CKIT-145-40XX PSoC® 4000S CapSense Prototyping Kit" for evaluating CapSense capability. 

It's working fine with code example "CE210709_CapSense_Linear_Slider_and_Buttons". But once I add a ADC block in the circuit, Build with error:  "Too many clocks allocated for CSD components. (App=cydsfit)"

Can 4054 have CapSense and ADC work together?

 

Thanks

0 Likes
1 Solution
Hari
Moderator
Moderator 750 replies posted 500 replies posted 250 solutions authored
Moderator

Hi @PatrickU 

 

The CapSense IP internally uses the ADC block, therefore, it is not possible to add another ADC along with CapSense in the same design. 

You need to use the CapSense_ADC component for achieving this. This is a separate component that you can obtain from the Component Catalog - 

Hari_0-1637898863937.png

 

This will let you configure ADC parameters as well and there is a dedicated tab within the CapSense_ADC configurator. 

Hari_1-1637898919612.png

 

Best regards, 
Hari

View solution in original post

0 Likes
2 Replies
Hari
Moderator
Moderator 750 replies posted 500 replies posted 250 solutions authored
Moderator

Hi @PatrickU 

 

The CapSense IP internally uses the ADC block, therefore, it is not possible to add another ADC along with CapSense in the same design. 

You need to use the CapSense_ADC component for achieving this. This is a separate component that you can obtain from the Component Catalog - 

Hari_0-1637898863937.png

 

This will let you configure ADC parameters as well and there is a dedicated tab within the CapSense_ADC configurator. 

Hari_1-1637898919612.png

 

Best regards, 
Hari

0 Likes
patrick1957
Level 1
First reply posted First question asked Welcome!
Level 1

It works now.

Thanks a lot

0 Likes