- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
we try to connect from cyble-022001-00 to 3 or 4 cyble-022001-00 successively.
First : we build a array ( TONOFFC [][] ) with the mac addresses we want to connect to.
Second : we read the address in the array and setup the peer address after that we connect.
Third : We disconnect the ble . This code is managed in other condition because that doesn't work if it is in the previous condition.
See below a part of our code :
Main ()
{
......
while (1)
....
{
peerAddr.bdAddr[0]=TONOFFC[intTest][5];
peerAddr.bdAddr[1]=TONOFFC[intTest][4];
peerAddr.bdAddr[2]=TONOFFC[intTest][3];
peerAddr.bdAddr[3]=TONOFFC[intTest][2];
peerAddr.bdAddr[4]=TONOFFC[intTest][1];
peerAddr.bdAddr[5]=TONOFFC[intTest][0];
peerAddr.type = 0;
CyBle_GapcConnectDevice(&peerAddr);
CyBle_ProcessEvents();
}
if(state==CONNECTED )
{
CyBle_GapDisconnect(cyBle_connHandle.bdHandle);
state=DISCONNECTED;
CyDelay(200u);
CyBle_ProcessEvents();
}
}
Result :
For the moment only the first device of the array is working. the while loop works correctly because each variable change.
But there is no connection to the second , third ... devices.
If somebody have any idea , please help us.
Nota : We already use this code for connect one cyble-022001-00 to another one and it works fine.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Are you not increamenting intTest variable in the code to select the necxt device.
Also please debug this by monitoring the return codes of the CyBle_GapcConnectDevice and CyBle_GapDisconnect APIs.
Also, keep looking for the CONNECT and DISCONNECT events in the callback handler
Regards,
-Madhu Sudhan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Are you not increamenting intTest variable in the code to select the necxt device.
Also please debug this by monitoring the return codes of the CyBle_GapcConnectDevice and CyBle_GapDisconnect APIs.
Also, keep looking for the CONNECT and DISCONNECT events in the callback handler
Regards,
-Madhu Sudhan