- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am using the CY8C4045AZI-S413 chip with 8 capsense buttons and i2c communication on pins p1.0 and p1.1. I want to use the CY8C4145AZI-S423 chip for the same and with the same pins but I do not know if it is possible.
The datasheet tells me this is possible, but then at the end of the datasheet it says that the CY8C4145AZI-S423 chip has no csd blocks and only 2 scb blocks. On this chip, the pins p1.0 and p1.1 can be used for i2c but in the scb[0] according to the datasheet. Can I use it? Or can only the scb[1] and scb[2] be used? I am trying to select those pins for i2c communication in PSoC Creator and it does not allow me, it only allows me the scb[1] and scb[2] blocks.
If someone can help me please!
Solved! Go to Solution.
- Labels:
-
PSoC 4 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @JoVa_4370637 ,
CY8C4145AZI-S423 Doesn't have CSD block so capsense is not supported
and P1[0] and P1[1] of CY8C4145AZI-S423 doesn't support I2C . So you cannot use the same pins for I2C.
Thanks,
Krupashankar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @JoVa_4370637 ,
CY8C4145AZI-S423 Doesn't have CSD block so capsense is not supported
and P1[0] and P1[1] of CY8C4145AZI-S423 doesn't support I2C . So you cannot use the same pins for I2C.
Thanks,
Krupashankar