Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
brza_3998571
Level 1
Level 1

I would like to use a mcu pin for capsense sensing as well as another sensor on the same pin. I would like to switch between what sensor I am reading from. I do see how to connect a capsense sensor to a analog mux sequencer if that is a possible solution.

0 Likes
1 Solution

Yes...external operation could be the best choice...

View solution in original post

0 Likes
3 Replies
RyanZhao
Moderator
Moderator
Moderator
250 sign-ins First question asked 750 replies posted

Hi Braeden,

Do you mean an external analog mux?  I think that depend on the resistance and capacitance char of the analog mux sequencer.

There is no routine inside the chip to use extra internal analog mux component.

Thanks,

Ryan

0 Likes

pastedImage_0.png

thanks for the response.

I am able to read each sensor on separate pins, but I would like to combine them onto the same pin using a mux like this so that I can choose which sensor I am reading from. I don't see how to connect a capsense sensor to something like this as there are no visible connections on the capsense block on the schematic.

So the only way to do this would be externally?

i am using a psoc 4200 series

0 Likes

Yes...external operation could be the best choice...

0 Likes