Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4

taghc_3472621
Level 1
Level 1

I am powering my CYBLE-214009-00 chip through a source selector. I believe when the source selector switches from one voltage source to the next, there is a voltage dip in the output voltage of the source selector (input VDD of my CYBLE chip) and the chip resets.

I want to stop this reset from happening, which is why I'm wondering if I can change the Brown Out Detection voltage somehow.

Open to any other suggestions.

Thanks

0 Likes
1 Solution
GyanC_36
Employee
100 likes received 50 likes received 25 likes received
Employee

Hi,

   I would recommend to use a cap as a solution for this issue. It is not possible/recommended to change the BOD voltage because it might cause the application corruption ( Flash etc) on operating at a voltage lower than the minimum operating voltage of chip.

-Gyan

View solution in original post

1 Reply
GyanC_36
Employee
100 likes received 50 likes received 25 likes received
Employee

Hi,

   I would recommend to use a cap as a solution for this issue. It is not possible/recommended to change the BOD voltage because it might cause the application corruption ( Flash etc) on operating at a voltage lower than the minimum operating voltage of chip.

-Gyan