cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

ALDE_1053476
New Contributor II

Hello,

I need to set up a BLE Link between two CYBLE-416045-02 Modules.

I need a 1 Mbit minimum (1.6 desired) Throughput.

Is it feasible?

Is there any example code available?

Thanks,

Alfonso

0 Likes
1 Solution
GeonaP_26
Moderator
Moderator

Apologies for the delay.

CYBLE-416045-02 contains PSoC 63 BLE device. Please refer to code example: CE222046 - PSoC 6 MCU with Bluetooth Low Energy (BLE) Connectivity: BLE Throughput Measurement which contains GATT server and client project. This client project measures the BLE data throughput and displays on a UART terminal emulator once in every 10 seconds.

View solution in original post

0 Likes
2 Replies
ALDE_1053476
New Contributor II

Hello,

Can anybody please answer my question?

Thanks,

Alfonso

0 Likes
GeonaP_26
Moderator
Moderator

Apologies for the delay.

CYBLE-416045-02 contains PSoC 63 BLE device. Please refer to code example: CE222046 - PSoC 6 MCU with Bluetooth Low Energy (BLE) Connectivity: BLE Throughput Measurement which contains GATT server and client project. This client project measures the BLE data throughput and displays on a UART terminal emulator once in every 10 seconds.

View solution in original post

0 Likes