- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I'm trying to get CYBLE-202007-EVAL to run Find Me Profile.
I plug the board into the CY8CKIT-042-BLE-A baseboard and communicate with CySmart.
But after connect for an hour, it just disconnect and the reason is CONNECT_TIMEOUT.
To extend range of BLE, I write the below code into file which I get from datasheet.
/* define the test register to switch the PA/LNA hardware control pins */
#define CYREG_SRSS_TST_DDFT_CTRL 0x40030008
/* Mandatory events to be handled by BLE application code */
case CYBLE_EVT_STACK_ON:
/* Configure the Link Layer to automatically switch PA control pin P3[2] and LNA control pin P3[3] */
CY_SET_XTND_REG32((void CYFAR *)(CYREG_BLE_BLESS_RF_CONFIG), 0x0331);
CY_SET_XTND_REG32((void CYFAR *)(CYREG_SRSS_TST_DDFT_CTRL), 0x80000302);
Does anyone have any ideas on this issue?
Thanks
Solved! Go to Solution.
- Labels:
-
BLE
-
ispn:39612:1:0
-
ispn:40070:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
You have to connect capacitor and Inductor which are named as C14 and L1 in the Module schematic to use the on board PCB antenna. Please refer the Module datasheet http://www.cypress.com/file/318881/download page #13 for schematic. Please go through the table placed near the UFL Connector at page#13 of above mentioned datasheet.
-Gyan