CYBLE-022001-00 OVTIO pins P5[0] and P5[1] not functioning as outputs
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
I cannot get pins 3 and 4 {P5[0] and P5[1]]) to function as digital outputs on the CYBLE-022001-00 BLE Module Development Board.

Is there something special that needs to be specified for these pins to work?

I have a simple project attached that toggles a single output pin at a 50mS rate.  On the Dev Board that I have, this project works on all I/O pins except P5[0] and P5[1], which are the OVTIO pins.

Thank you.

0 Likes
1 Solution
SayaniS_66
Moderator
Moderator
Moderator
10 likes received First like received

Hello,

Can you please elaborate your test scenario. We tested your project with pin set to P5.0 and P5.1 and checked the output on an oscilloscope. Both the pins are working correctly as digital output pin.

-Sayani.

View solution in original post

0 Likes
2 Replies
SayaniS_66
Moderator
Moderator
Moderator
10 likes received First like received

Hello,

Can you please elaborate your test scenario. We tested your project with pin set to P5.0 and P5.1 and checked the output on an oscilloscope. Both the pins are working correctly as digital output pin.

-Sayani.

0 Likes
Anonymous
Not applicable

Okay.

I have ordered a new Eval board already.

I should have it Monday.

Thank You.

Scott Coleman

949-289-1578

0 Likes