The CY8CKIT-142 module communicates and runs the test firmware ok when mounted on the CY8CKIT-042 BLE KIT. When I place it on my own baseboard, the CYsmart application does not see the module. On the custom designed baseboard, I am providing 5 volts and ground connections to VDDD and the module GND. When the module is installed on the custom baseboard, I can measure 5 volts on VDDD, VDDA and VDDR. What other pins should I supply with voltages?. I measured a 3.3 volt on J10 pin 15 (P2_6) and 4 volts on J11 pin 12 (P1_4) on the BLE kit without the module connected.
Solved! Go to Solution.
You have also addressed the attached pic config on your custom board (from the 042 BLE
manual).
Regards, Dana.
Apart from that, lok at the schematic that is in the -042 kit users guide. There you can see all the connections from the base board to the module. But I used the module on a custom baseboard by myself, and providing proper voltage (3.3V for me) was enough.
ok, thank you. I solved the problem.
ok, thank you. I solved the problem.