Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

tk1
Level 1
Level 1
First like received 25 sign-ins First solution authored

CY8CKIT-041S-MAX 

How to connect a sensor to the header of the main board

0 Likes
1 Solution

Hi, @tk1 


I researched the pins you want to place the sensors on and it appears they are already assigned to the evaluation touchpad, slider, and buttons.
You can open up the pins that are already assigned, but it would be difficult to assign them to the pins (J1, J2, J3, J6, J4) on the main board because of the wiring pattern.
Therefore, as far as I know, the only way to extend the 40-pin connector is to use a board like the link.

https://akizukidenshi.com/catalog/g/gP-10187/

I hope this helps you.

 

Best Regards,

Chihiro Tatebayashi 

View solution in original post

0 Likes
8 Replies
NXTY_Tatebayasi
Level 4
Level 4
5 solutions authored 25 replies posted 100 sign-ins

Hi,

What is the sensor you want to connect to that board?

 

Regards,

Chihiro Tatebayashi

0 Likes
tk1
Level 1
Level 1
First like received 25 sign-ins First solution authored

外部タッチボタン一つです

0 Likes
tk1
Level 1
Level 1
First like received 25 sign-ins First solution authored

I want to know how to connect one external electrostatic sensor to the Expansion Headers of the Pioneer Board of CY8CKIT-041S-MAX.

0 Likes
ncbs
Moderator
Moderator
Moderator
500 replies posted 50 likes received 250 sign-ins

Hi @tk1 ,

I would suggest you go through the datasheet of the "electrostatic sensor", and connect the sensor to the GPIOs of the S-MAX kit. If the GPIOs need to be configured as special-purpose pins, specific GPIOs need to be configured. You may find detailed information in section 3.1 Alternate pin functions of the datasheet.

Regards,
Nikhil

0 Likes
NXTY_Tatebayasi
Level 4
Level 4
5 solutions authored 25 replies posted 100 sign-ins

Hi, @tk1

You can assign a Capsense sensor to any of the GPIOs from the tool.

Capsense can be connected to the pins corresponding to MSC_SENSE described in the datasheet.

The tool uses the capsense configurator. You can either auto assign or manually specify the pins.

For more information, we recommend referring to the ModusToolbox™ CAPSENSE™ Configurator user guide.

And for a touch one button,I guess you can carry out your project by using the capsense configrator to change the capsense pin assignment assigned to the sample code here.

I wish you the best !

 

PSoC4 msc-capsense-csd-button-tuning.git 

PSoC 4100S Max DataSheet 

ModusToolbox CAPSENSE Configurator 5.0 User Guide 

 

Best Regards,

Chihiro Tatebayashi

0 Likes
tk1
Level 1
Level 1
First like received 25 sign-ins First solution authored

thank you

I want to insert a pin somewhere on J1, J2, J3, J6, J4 on the main board and make one touch sensor.
When I try to configure with Capsense configurator, Device Configurator
Settings cannot be made with the terminals on the main board.
Only pin numbers on the SENSING Expansion Board can be set.
Is it possible to do it with any pin of J1, J2, J3, J6, J4 on the main board?
I want to know how to set it.

Hi, @tk1 


I researched the pins you want to place the sensors on and it appears they are already assigned to the evaluation touchpad, slider, and buttons.
You can open up the pins that are already assigned, but it would be difficult to assign them to the pins (J1, J2, J3, J6, J4) on the main board because of the wiring pattern.
Therefore, as far as I know, the only way to extend the 40-pin connector is to use a board like the link.

https://akizukidenshi.com/catalog/g/gP-10187/

I hope this helps you.

 

Best Regards,

Chihiro Tatebayashi 

0 Likes
tk1
Level 1
Level 1
First like received 25 sign-ins First solution authored

thank you

0 Likes
This widget could not be displayed.