PSoC™ 4 Forum Discussions
hello, we develop a project with CY8C 4149 and project go very well, we switch the chip cy8c4149 to cy8c4148 and program cyc84148, it got failure. we understand the cy8c4148 has flash memory of 256kb, our firmware size is 235kb, it should allow to be programmed in cy8c4148. following image is the programmer programming result.
Could you help me out to successfully program in cy8c4148
Thank you
Show LessHi 我试着新建一个空工程,添加一个button,但发现编译时,cycfg_capsense.h这个头文件没有调用成功,请帮忙看一下是什么问题?谢谢
Dear community,
Working on a project based on CY8C4046LQI-T452 reached the stage where we need to think on the production automation and more specifically on the chip programming. For my great disappointment, there seems to be no options to do a CLI programming using the cheaper(KitProg3) option. From what I have read, reached to the following conclusion:
-Modus Toolbox CLI is not suitable as the make/build option is not desired
-PSoC Programmer does not support the target and is not going to
-mtb-programmer does not have CLI option
The last option left is using a J-Link.
Would appreciate you suggestions
Kind regards
ST
Hi, Teams.
I have a question.
Can you support CY8CKIT-002 for WIN11?
If it can be used, what is the difference in functionality from MiniProg4?
Best Regarsds, Haru
Show Less请问一下,就是我用PSOC4芯片来设计一个信号发生器,那么我应该用什么软件去进行一个仿真,就比如我没有示波器的实物,但是如果我用labview做了一个虚拟示波器,如何用这个虚拟示波器来显示我用PSOC设计的这个DDS信号发生器的功能呢?
Hi,
I am doing a research project using CY8CKIT-042 PSoC4 Pioneer Kit (CY8C4245AXI-483). The prototype device is powered from a battery of 40mAh capacity. After the normal mode operation when I power OFF the device, the uC enters into deep sleep power saving mode. From the deep sleep mode when I connect charger for charging the battery or press the power ON key then uC exits from deep sleep mode and enters into normal mode.
However in an extreme case, the battery was weak while the time I powered OFF the device then in between the deep sleep operation state the battery was fully drained and there was no power source to the device and uC wad fully turned OFF.
After the above scenario, when I connect a power source to the device the expected behaviour is that the device should turn ON automatically due to the reset signal that appears on connecting the power source. However, in some scenario the device didn't turned ON and a re-flashing of the uC was required for turning ON and resuming the expected behaviour.
Can anyone suggest some root cause for this behaviour and what could the possible solution to avoid it?
Thanks in advance.
Show LessI tried coneccting CySmart 1.3.0.8 and CY8CKIT-042-BLE-A using default settings.
Then, too many peer devices were listed in master tab.
Could I delete peer devices from list when I push [start scan]?
and is there a way to display only Cypress(Infineon) devices on master tab?
Or Could I serch and sort devices with device name?
best regards
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/PSoC-4/CySmart-configuration/td-p/741035
Show Lesshi, Im music developer try to create new instrument basic on Eastern instrument ,i start my prototype with Arduino board .
I want to change for Infineon microprocessor ,I need same touchkeys function in this link .
- different dimensions keys board
- Bluetooth MIDI/OSC transmit messages controller
- 156 touch switch
- 26 touch keys with full midi/osc controller function
-OLED display
((My main question is which microprocessor i need to start with .))
Show Less
Hello together,
in the description of the HSIOM_AMUX_SPLIT_CTL-Registers I found that there seems to be a switch to connect the Bus to GND/VSSA. The switch is named SWITCH_AA_S0 (or BB for Bus B). In one of my application it would be helpful to use this switch to discharge the whole bus.
Is there any documentation how this switch works? I tried to activate it, but I didn't see any success.
Unfortunately I did not find any details in the TRM for PSoC4100PS. Also I can't find any details in the code or in the analog routing graphics.
Br,
Pascal
Show Less