- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I have the CY8CKIT-042-BLE kit and have used the CY5670 dongle with CySmart 1.2 and it has been very useful. Now suddenly CySmart won't see the dongle. It brings up a dialog that says I have to update the firmware to C:\Program Files(x86)\Cypress\Cysmart1.2\dongle\CY5670\BLE_4_1_Dongle_CySmart_128K.hex.
But when I open PSoc Programmer 3.24.2 It says the dongle is running that file. (see PNG attached)
Successfully Connected to KitProg/BLE0F20122F03314400 at 4:32:11 AM | KitProg Version 2.16
Opening Port at 4:32:10 AM |
Device set to CYBL10162-56LQXI at 4:32:09 AM | 131072 FLASH bytes
Device Family set to CY8C4xxx-BLE at 4:32:09 AM |
Active HEX file set at 4:32:09 AM | C:\Program Files (x86)\Cypress\CySmart\1.2\dongle\CY5670\BLE_4_1_Dongle_CySmart_128K.hex
|
| Users must be aware that the following PSoC device should not be powered or programmed at 5V. Doing so will cause damage to the device: CYRF89xxx
Session Started at 4:32:08 AM | PPCOM Version 20.0
So it has the correct file but still won't use it. All my Cypress programs have been updated to current, Any suggestions what I can do ?
Thank you,
--jim schimpf
Solved! Go to Solution.
- Labels:
-
BLE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Probably you mix two different resources needed:
The Kitprog which seemingly is up-to-date
and the firmware. You can see which hex-file to be programmed is selected, but you cannot see that the file has been programmed.
Bob