Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

ThBi_3905606
Level 2
Level 2
10 replies posted 10 questions asked 10 sign-ins

Hello,

I use a CY3280MBR3 to rate the CY8CMBR3116,

I use an arduino as a host.

my sketch is very simple, for every touch detected I send MIDI notes

I have a very bad times responses: 78 - 80 ms.

If a try my timing test before I2C communication, I have 77 ms between the trig sensor and the interrupt pin signal.

In the software the initial response times says 80 ms and the subsequent response time 60 ms.

there is a way to have more fast responses, the datasheet say 20 ms scanning times; why the interrupt pin signal arrive 77ms after the trig ?

Thomas

1 Solution
Vison_Zhang
Moderator
Moderator
Moderator
250 sign-ins 250 solutions authored 10 likes given

You can try to set the debounce to 1, when debounce =3, a sensor won't be triggered until it is detected  for 3 consecutive scan cycles.

View solution in original post

0 Likes
1 Reply
Vison_Zhang
Moderator
Moderator
Moderator
250 sign-ins 250 solutions authored 10 likes given

You can try to set the debounce to 1, when debounce =3, a sensor won't be triggered until it is detected  for 3 consecutive scan cycles.

0 Likes