Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

I'm now on design/schematic-phase for the CY8C4024LQI-S411 - based on above mentioned program-example (but with 9 buttons).

The Pin-configuration I have chosen as follow:

pastedImage_2.png

Now I'm not sure, if I need to connect wco_in and wco_out to capacitors because above mentioned program is using the watchdog??

pastedImage_0.png

also I'm not sure about follow capacitor see below, does I need it?:

pastedImage_3.png

thank you very much

0 Likes
1 Solution
BrandonP_16
Employee
Employee
5 sign-ins First question asked 10 solutions authored

Hi,

CY8C4024LQI-S411(PSoC4S) device can work watchdog without WCO. If you do not want to mount WCO, you can ignore C9/C12 capacitors.

Also, C3 capacitor does not used for CapSense operation or watchdog.

Thanks,

Brandon

View solution in original post

0 Likes
2 Replies
BrandonP_16
Employee
Employee
5 sign-ins First question asked 10 solutions authored

Hi,

CY8C4024LQI-S411(PSoC4S) device can work watchdog without WCO. If you do not want to mount WCO, you can ignore C9/C12 capacitors.

Also, C3 capacitor does not used for CapSense operation or watchdog.

Thanks,

Brandon

0 Likes
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

The WCO in the PSoC4000s has the only one function: to trim IMO, higher the accuracy from 2% to 0.2%.

The inner clock ILO is the source clock of WDT.

So it is Ok to use P0.4 and P0.5 as the capsense pins.

In addition, you don't need to populate the bypass capacitor on this kit as this is intended for future use.

0 Likes