- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello.
I am new to the Cypress Developer Community.
I recently purchased the CY8CKIT-042-BLE-A Bluetooth Low Energy Kit, for a work related project.
I am using the CY5670: CySmart USB Dongle as a Master, to receive and log RSSI data from the CYBLE-022001-00 EZ-BLE PRoC Module.
After establishing connection to a device, the CySmart 1.2 desktop tool is used to manually log RSSI data, using the <Get RSSI> command, found on the send command’s tab.
How can this process be automated, without having to manually send the <Get RSSI> repeatedly?
The data logging requirement is to read 10 values of <Get RSSI> every 5 minutes, for a period of 3 hours.
Your insight will be highly appreciated.
I have attached a word document, for a screen capture of the CySmart 1.2 gui, set up, if that helps
Regards,
Andrew
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Well, if you have the CySmart source code, you can modify it to log for 2/min for 3 hours when you click a button. But, I don't think the CySmart code is open for use, so you might have better luck with the mobile phone app cysmart code: http://www.cypress.com/documentation/software-and-drivers/cysmart-mobile-app
There is code for both the iOS and the Android platforms, but the windows version is absent.
Basically modify it to query the RSSI and write the data to a file for 360 iterations at once per 30 seconds. You will need to write the program/functionality yourself unfortunately